You are viewing documentation for version:
Structure to hold the threshold detection configuration parameters. 
Public Attributes#
uint8_t *
Condition for Threshold 1 (for example, Equal, Greater, Lesser). 
uint8_t *
Condition for Threshold 2 (for example, Equal, Greater, Lesser). 
Public Attribute Documentation#
threshold1#
uint16_t sl_adc_threshold_config_t::threshold1
Threshold 1 value. 
threshold2#
uint16_t sl_adc_threshold_config_t::threshold2
Threshold 2 value. 
threshold1_cond#
uint8_t* sl_adc_threshold_config_t::threshold1_cond
Condition for Threshold 1 (for example, Equal, Greater, Lesser). 
threshold2_cond#
uint8_t* sl_adc_threshold_config_t::threshold2_cond
Condition for Threshold 2 (for example, Equal, Greater, Lesser). 
range#
uint8_t sl_adc_threshold_config_t::range
Range of the threshold.