Structure representing the response for reading the maximum data length in BLE.
Public Attribute Documentation#
maxtxoctets#
uint16_t rsi_ble_resp_read_max_data_length_s::maxtxoctets
maxtxoctets
- Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection. 
maxtxtime#
uint16_t rsi_ble_resp_read_max_data_length_s::maxtxtime
maxtxtime
- Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection 
maxrxoctets#
uint16_t rsi_ble_resp_read_max_data_length_s::maxrxoctets
maxrxoctets
- Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection 
maxrxtime#
uint16_t rsi_ble_resp_read_max_data_length_s::maxrxtime
maxrxtime
- Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.