Union representing the value of the UUID. This union stores the value of the UUID, which can be of three different sizes: 128-bit, 32-bit, or 16-bit. The appropriate field in the union should be used depending on the size of the UUID.
Public Attribute Documentation#
val128#
uuid128_t uuid_s::uuid_t::val128
128-bit UUID value. uuid128_t
This member holds the value of a 128-bit UUID, which is divided into four segments:
- The first 32 bits ( - data1)
- The next 16 bits ( - data2)
- The following 16 bits ( - data3)
- The final 64 bits ( - data4), stored as an array of 8 bytes
These segments together represent a full 128-bit UUID, compliant with the standard UUID format.
val32#
uuid32_t uuid_s::uuid_t::val32
32-bit UUID value. This field holds the value of a 32-bit UUID, stored as an array of 4 bytes.
val16#
uuid16_t uuid_s::uuid_t::val16
16-bit UUID value. This field holds the value of a 16-bit UUID, stored as an array of 2 bytes.