Structure representing a Wi-Fi buffer.
Public Attributes#
sl_slist_node_t
Pointer to the node of the list of which the buffer is part of.
uint32_t
Size of the buffer in bytes.
uint8_t
Indicates the buffer type (SL_WIFI_TX_FRAME_BUFFER, SL_WIFI_RX_FRAME_BUFFER, and so on) corresponding to the buffer.
uint8_t
Buffer identifier. Can be used to uniquely identify a buffer. Loops every 256 packets.
uint8_t
Reserved.
uint8_t
Stores the data (header + payload) to be sent to NWP.
Public Attribute Documentation#
node#
sl_slist_node_t sl_wifi_buffer_t::node
Pointer to the node of the list of which the buffer is part of.
type#
uint8_t sl_wifi_buffer_t::type
Indicates the buffer type (SL_WIFI_TX_FRAME_BUFFER, SL_WIFI_RX_FRAME_BUFFER, and so on) corresponding to the buffer.
id#
uint8_t sl_wifi_buffer_t::id
Buffer identifier. Can be used to uniquely identify a buffer. Loops every 256 packets.