Hardware Overview#
Hardware Platform#
The flash programmer supports two hardware topologies: one which is based on the SiWx917 Pro Kit and the other which is based on a custom hardware design. These are described in the following sections.
SiWx917 Pro Kit#
The SiWx917 Pro Kit consists of a radio board and a mainboard.
The radio board supports on-chip antenna and micro-coaxial connector for conducted RF measurements or external antenna connection
Virtual COM port
SEGGER J-link on-board debugger
Breakout pads for Wireless SoC I/O
The flash programmer uses the SEGGER J-link on-board debugger for communicating with the SiWx917 SoC.
Customized Hardware#
Alternatively, the SiWx917 SoC device can be used on a custom hardware platform to implement the programmer.
The SWDIO and SWCLK pins are used by SWD.
The SWD pins can be used to communicate with the SWD Programmer.