Functions#

This section provides a reference to the AES Crypto API Functions.

Functions#

sl_status_t
sl_si91x_aes(sl_si91x_aes_config_t *config, uint8_t *output)

To encrypt or decrypt the message according to the given configuration.

sl_status_t
sl_si91x_aes_multipart(const sl_si91x_aes_config_t *config, uint16_t chunk_length, uint8_t aes_flags, uint8_t *output)

Encrypts or decrypts a chunk of a message according to the given configuration.

Function Documentation#

sl_si91x_aes#

sl_status_t sl_si91x_aes (sl_si91x_aes_config_t * config, uint8_t * output)

To encrypt or decrypt the message according to the given configuration.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_aes_config_t *[in]config

Configuration object of type sl_si91x_aes_config_t

uint8_t *[out]output

Buffer to store the output.

This is a blocking API. Note

  • The maximum length of the message in bytes that can be handled in one go is determined by SLI_SI91X_MAX_DATA_SIZE_IN_BYTES_FOR_AES. If the message length is not a multiple of SL_SI91X_AES_BLOCK_SIZE, the function returns an error.

Returns


sl_si91x_aes_multipart#

sl_status_t sl_si91x_aes_multipart (const sl_si91x_aes_config_t * config, uint16_t chunk_length, uint8_t aes_flags, uint8_t * output)

Encrypts or decrypts a chunk of a message according to the given configuration.

Parameters
TypeDirectionArgument NameDescription
const sl_si91x_aes_config_t *[in]config

Configuration object of type sl_si91x_aes_config_t containing the AES operation parameters.

uint16_t[in]chunk_length

Length of the current chunk to be processed in bytes.

uint8_t[in]aes_flags

Flags indicating the position of the current chunk. Valid values are:- SL_SI91X_AES_FIRST_CHUNK, SL_SI91X_AES_MIDDLE_CHUNK, SL_SI91X_AES_LAST_CHUNK. Buffer to store the processed output data.

uint8_t *N/Aoutput

This is a blocking API. Returns

Note

    • The maximum length of the message in bytes that can be handled in one go is determined by SLI_SI91X_MAX_DATA_SIZE_IN_BYTES_FOR_AES.

    • If the message length exceeds this limit, the function returns SL_STATUS_INVALID_PARAMETER.

    • If the message length is not a multiple of SL_SI91X_AES_BLOCK_SIZE, the function returns an error.