Wi-Fi Management Frame Protection (MFP) configuration structure.

This structure is used to configure the MFP mode for Wi-Fi operations. It includes the MFP mode and a flag indicating whether the MFP mode is explicitly configured or automatically detected. Members:

  • mfp_mode: MFP mode setting of type sl_wifi_mfp_mode_t

  • is_configured: True if MFP mode is explicitly configured, false for automatic detection.

  • reserved: Reserved for future use and alignment.

Public Attributes#

bool

True if MFP mode is explicitly configured, false for automatic detection.

uint8_t

Reserved for future use and alignment.

Public Attribute Documentation#

mfp_mode#

sl_wifi_mfp_mode_t sl_wifi_mfp_config_t::mfp_mode

MFP mode setting of type sl_wifi_mfp_mode_t.


is_configured#

bool sl_wifi_mfp_config_t::is_configured

True if MFP mode is explicitly configured, false for automatic detection.


reserved#

uint8_t sl_wifi_mfp_config_t::reserved[2]

Reserved for future use and alignment.