You are viewing documentation for version:
Wi-Fi Request to Send (RTS) threshold structure.
This structure is used to configure the RTS threshold for Wi-Fi operations.
Members:
rts_threshold: RTS threshold in bytes. The device performs an RTS/CTS handshake when the packet size exceeds the threshold.
reserved: Reserved fields for future use, should be set to zero.
Public Attributes#
uint16_t
Request to Send (RTS) threshold in bytes.
Public Attribute Documentation#
rts_threshold#
uint16_t sl_wifi_rts_threshold_t::rts_threshold
Request to Send (RTS) threshold in bytes.
reserved#
uint8_t sl_wifi_rts_threshold_t::reserved[2]
Reserved fields.