Button#

Introduction#

The SI91x button driver is a platform-level software module designed to manage button initialization and reading. It provides a wide range of functions for handling button operations, such as initialization, state monitoring, and callback management for state changes. The driver supports flexible interrupt configurations, allowing detection based on button state, edge transitions, or a combination of both. All button functions are accessed via the generic driver, which internally calls specific functions for the corresponding button.

Configuration#

All button instances are configured using the sl_button_t struct. This struct along with a function definition for initializing Button is automatically generated when an Button is set up using Simplicity Studio's wizard. This struct sl_button_t struct is automatically generated into the following files sl_si91x_button_instances.h and sl_si91x_button_instances.c. The samples below are for a single instance called "btn0".

// sl_si91x_button_instances.c
#include "sl_si91x_button_pin_config.h"
#include "sl_si91x_button_instances.h"
#include "sl_si91x_button_btn0_config.h"

sl_button_t const button_btn0 = {
  .port = SL_BUTTON_BTN0_PORT,
  .pin = SL_BUTTON_BTN0_PIN,
  .button_number = SL_BUTTON_BTN0_NUMBER,
  #ifdef SL_BUTTON_BTN0_PAD
  .pad = SL_BUTTON_BTN0_PAD,
  #endif
  .interrupt_config = SL_BUTTON_CONFIG_BTN0_INTR
};

void button_init_instances(void)
{
  sl_si91x_button_init(&button_btn0);
}

Note

  • The sl_si91x_button_instances.c file is shown with only one instance, but if more were in use they would all appear in this .c file.

// sl_si91x_button_instances.h
#ifndef SL_SI91X_BUTTON_INSTANCES_H
#define SL_SI91X_BUTTON_INSTANCES_H

#include "sl_si91x_button.h"

extern const sl_button_t button_btn0;


void button_init_instances(void);
void sl_simple_button_init_instances(void);

#endif // BUTTON_INSTANCES_H

Note

  • The sl_si91x_button_instances.h file is shown with only one instance, but if more were in use they would all appear in this .h file.

  • For more information on configuring available parameters, see the respective peripheral example readme document and Peripheral Configuration.

Usage#

After the button structures are defined, button functions can be called by passing an instance of sl_button_t, which will internally redirect to the type-specific version of the function. The commonly used functions include the following:

  1. To initialize the button: sl_si91x_button_init

  2. To return the current state (pressed or released) of the pin associated with a button: sl_si91x_button_state

  3. To toggle the value of a local variable associated with the state of button: sl_si91x_button_toggle_state

  4. A callback that user can modify for the application: sl_si91x_button_isr

The sl_si91x_button_init function is automatically invoked when the application starts.

The button driver supports interrupt mode, with or without debounce functionality.The application can implement sl_si91x_button_state to determine the current state of the button when needed. Additionally, sl_si91x_button_toggle_state can be implemented by the application to toggle the "soft" state, enabling interrupts and their callbacks. The sl_si91x_button_isr is a callback function triggered by a change in the button's state, and the application can implement this function to define the desired actions upon a state change.

Modules#

sl_button_t

Macros#

A set of numerical macros for use with the button APIs.

#define
HIGH_LEVEL_INTERRUPT SL_GPIO_INTERRUPT_HIGH

To configure or to trigger the interrupt based on logic levels (LOW, HIGH, or both) or edge changes (rising, falling, or both).

#define
LOW_LEVEL_INTERRUPT SL_GPIO_INTERRUPT_LOW

Interrupt on level low/pressed button state can be configured.

#define

Interrupt on level low/pressed and high/released button state can be configured.

#define
RISE_EDGE_INTERRUPT SL_GPIO_INTERRUPT_RISING_EDGE

Interrupt on level rising edge of the button press.

#define
FALL_EDGE_INTERRUPT SL_GPIO_INTERRUPT_FALLING_EDGE

Interrupt on level falling edge of the button press.

#define
RISE_EDGE_AND_FALL_EDGE_INTERRUPT SL_GPIO_INTERRUPT_RISE_FALL_EDGE

Interrupt on level rising edge and falling edge of the button press.

#define

Button state is pressed.

#define

Button state is released.

#define

Button state is invalid.

Functions#

void
sl_si91x_button_init(const sl_button_t *handle)

To initialize the specified button with the given configuration.

sl_status_t
sl_si91x_button_deinit(const sl_button_t *handle)

Deinitialize the specified button and release associated resources.

void
sl_si91x_button_isr(uint8_t pin, int8_t state)

To handle the interrupt when a button changes its state.

uint8_t
sl_si91x_button_get_state(uint8_t button_number)

To get the current state (pressed or released) of a button.

uint8_t
sl_si91x_button_state(uint8_t pin, uint8_t port)

To return the current state (pressed or released) of the pin associated with a button.

void
sl_si91x_button_toggle_state(uint8_t button_number)

To toggle the value of a local variable associated with the state of a button.

void
sl_si91x_button_set_state(uint8_t button_number, int8_t state)

To set the state (pressed or released) of the pin associated with a button.

int8_t

Older API - Not recommended to use.

int8_t

Older API - Not recommended to use.

void

Older API - Not recommended to use.

void
sl_si91x_button_state_set(uint8_t pin, int8_t state)

Older API - Not recommended to use.

Macros Documentation#

HIGH_LEVEL_INTERRUPT#

#define HIGH_LEVEL_INTERRUPT
Value:
SL_GPIO_INTERRUPT_HIGH

To configure or to trigger the interrupt based on logic levels (LOW, HIGH, or both) or edge changes (rising, falling, or both).

Interrupt on level high/released button state.


LOW_LEVEL_INTERRUPT#

#define LOW_LEVEL_INTERRUPT
Value:
SL_GPIO_INTERRUPT_LOW

Interrupt on level low/pressed button state can be configured.


HIGH_LEVEL_AND_LOW_LEVEL_INTERRUPT#

#define HIGH_LEVEL_AND_LOW_LEVEL_INTERRUPT
Value:
(HIGH_LEVEL_INTERRUPT \
| LOW_LEVEL_INTERRUPT)

Interrupt on level low/pressed and high/released button state can be configured.


RISE_EDGE_INTERRUPT#

#define RISE_EDGE_INTERRUPT
Value:
SL_GPIO_INTERRUPT_RISING_EDGE

Interrupt on level rising edge of the button press.


FALL_EDGE_INTERRUPT#

#define FALL_EDGE_INTERRUPT
Value:
SL_GPIO_INTERRUPT_FALLING_EDGE

Interrupt on level falling edge of the button press.


RISE_EDGE_AND_FALL_EDGE_INTERRUPT#

#define RISE_EDGE_AND_FALL_EDGE_INTERRUPT
Value:
  SL_GPIO_INTERRUPT_RISE_FALL_EDGE

Interrupt on level rising edge and falling edge of the button press.


BUTTON_PRESSED#

#define BUTTON_PRESSED
Value:
1

Button state is pressed.


BUTTON_RELEASED#

#define BUTTON_RELEASED
Value:
0

Button state is released.


BUTTON_STATE_INVALID#

#define BUTTON_STATE_INVALID
Value:
-1

Button state is invalid.


Function Documentation#

sl_si91x_button_init#

void sl_si91x_button_init (const sl_button_t * handle)

To initialize the specified button with the given configuration.

Parameters
TypeDirectionArgument NameDescription
const sl_button_t *[in]handle

Pointer to an sl_button_t button configuration structure containing the specific button details.

This function configures the GPIO settings and interrupt configurations for the specified button. It handles different configurations based on the board version and button number. For UULP (Ultra-Low Power) and M4 (High-Performance) GPIOs, it sets the pin direction, pin mode, and interrupt settings.

  • The button configuration structure must be properly initialized before calling this function.

  • The specified button will be configured and ready for use with the specified settings.

Note

  • This function handles different configurations based on the board version and button number. For UULP (Ultra-Low Power) and M4 (High-Performance) GPIOs, it sets the pin direction, pin mode, and interrupt settings.


sl_si91x_button_deinit#

sl_status_t sl_si91x_button_deinit (const sl_button_t * handle)

Deinitialize the specified button and release associated resources.

Parameters
TypeDirectionArgument NameDescription
const sl_button_t *[in]handle

Pointer to an sl_button_t structure containing the button configuration details.

This function deinitializes the specified button. After deinitialization, the button is no longer functional until reinitialized.

Returns

  • sl_status_t Status of the operation:

    • SL_STATUS_OK if the button was successfully deinitialized.

    • SL_STATUS_INVALID_HANDLE if the button number is invalid.

Note

  • This function handles deinitialization for HP (High-Performance), ULP and UULP buttons.


sl_si91x_button_isr#

void sl_si91x_button_isr (uint8_t pin, int8_t state)

To handle the interrupt when a button changes its state.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The button pin which has changed state, either BUTTON0 pin or BUTTON1 pin as defined.

int8_t[in]state

The new state of the button referenced by the button parameter, either BUTTON_PRESSED if the button has been pressed or BUTTON_RELEASED if the button has been released.

This callback is called in the interrupt context whenever a button changes its state. It must be implemented by the application to handle the functionality in response to the button state change.

Note

  • This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.


sl_si91x_button_get_state#

uint8_t sl_si91x_button_get_state (uint8_t button_number)

To get the current state (pressed or released) of a button.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]button_number

The button number being queried.

This function returns the shadow state of the button rather than reading the actual state of the pin. It is correlated with the interrupts and their callbacks, providing a "soft" state.

Returns


sl_si91x_button_state#

uint8_t sl_si91x_button_state (uint8_t pin, uint8_t port)

To return the current state (pressed or released) of the pin associated with a button.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The button pin being queried

uint8_t[in]port

The button port being queried

This function reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.

Returns


sl_si91x_button_toggle_state#

void sl_si91x_button_toggle_state (uint8_t button_number)

To toggle the value of a local variable associated with the state of a button.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]button_number

The button number being queried.

This function toggles the state of a local variable that tracks the state of the specified button. It must be implemented by the application to handle the functionality in response to the button state change.

Note

  • This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.


sl_si91x_button_set_state#

void sl_si91x_button_set_state (uint8_t button_number, int8_t state)

To set the state (pressed or released) of the pin associated with a button.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]button_number

The button number being queried.

int8_t[in]state

The state of the button to be set:

This function sets the state of the specified button pin. It must be implemented by the application to handle the functionality in response to changes of state in each of the buttons or callbacks to the appropriate functionality.

Note

  • This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.


sl_si91x_button_state_get#

int8_t sl_si91x_button_state_get (uint8_t pin)

Older API - Not recommended to use.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The button pin being queried, either SL_BUTTON_BTN0_PIN or SL_BUTTON_BTN1_PIN as defined.

This function returns the shadow state of the button rather than reading the actual state of the pin. It is correlated with the interrupts and their callbacks, providing a "soft" state.

Returns

Note

  • This function is deprecated and should be replaced with sl_si91x_button_get_state.


sl_si91x_button_pin_state#

int8_t sl_si91x_button_pin_state (uint8_t pin)

Older API - Not recommended to use.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The button pin being queried, either BUTTON0 pin or BUTTON1 pin as defined.

This function reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.

Returns

Note

  • This function is deprecated and should be replaced with sl_si91x_button_state.


sl_si91x_button_state_toggle#

void sl_si91x_button_state_toggle (uint8_t pin)

Older API - Not recommended to use.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The button pin which has changed state, either BUTTON0 pin or BUTTON1 pin as defined.

This function toggles the state of a local variable that tracks the state of the specified button. It must be implemented by the application to handle the functionality in response to the button state change.

Note

  • This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.

Note

  • This function is deprecated and should be replaced with sl_si91x_button_toggle_state.


sl_si91x_button_state_set#

void sl_si91x_button_state_set (uint8_t pin, int8_t state)

Older API - Not recommended to use.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The button pin which has changed state, either BUTTON0 pin or BUTTON1 pin as defined.

int8_t[in]state

The state of the button to be set:

This function sets the state of the specified button pin. It must be implemented by the application to handle the functionality in response to changes of state in each of the buttons or callbacks to the appropriate functionality.

Note

  • This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.

Note

  • This function is deprecated and should be replaced with sl_si91x_button_set_state.