Structure representing the BLE start encryption request.

This structure is used to define the parameters for a BLE start encryption request, which includes the address of the connected device, the remote device's Encrypted Diversifier (EDIV) value, Random (RAND) value, and Long Term Key (LTK) value.

Public Attributes#

uint8_t
uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_start_encryption_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the connected device


ediv#

uint16_t rsi_ble_start_encryption_s::ediv

Remote device EDIV value


rand#

uint8_t rsi_ble_start_encryption_s::rand[RSI_BLE_RAND_LEN]

Remote device RAND value


ltk#

uint8_t rsi_ble_start_encryption_s::ltk[RSI_BLE_ENC_KEY_LENGTH]

Remote device LTK value