Event Types#
This section provides a reference to Bluetooth Low Energy (BLE) API events.
Modules#
rsi_ble_event_enhnace_conn_status_s
rsi_ble_event_le_ping_time_expired_s
rsi_bt_event_le_security_keys_s
rsi_bt_event_encryption_enabled_s
rsi_bt_event_smp_passkey_display_s
rsi_ble_event_remote_conn_param_req_s
rsi_ble_event_remote_features_s
rsi_ble_event_le_dev_buf_ind_s
rsi_ble_event_data_length_update_s
rsi_ble_event_profile_by_uuid_s
rsi_ble_resp_query_profile_descriptor_s
rsi_ble_resp_local_att_value_s
rsi_ble_event_remote_device_info_s
rsi_ble_event_mtu_exchange_information_s
rsi_ble_event_directedadv_report_s
rsi_ble_event_cbfc_conn_complete_s
rsi_bt_event_controller_logs_s
Typedefs#
Structure representing an advertising report event.
Structure representing the connection status event in the module.
Structure representing the enhanced connection status event in the module.
Disconnection event structure.
The structure represents the LE ping timeout expired event.
The structure represents the Long Term Key (LTK) request event.
The structure represents security keys event.
Structure to hold the event data for encryption enabled event.
Structure to hold the Security Manager Protocol (SMP) request event.
Structure to hold the SMP response event data.
Structure to hold the SMP passkey event data.
Structure to hold the SMP passkey display event.
Structure to hold the Secure Connections (SC) passkey event.
Structure to hold the information related to Security Manager Protocol (SMP) failed event.
Structure to define the Bluetooth event security method.
Structure representing the event for Cross Transport Key Derivation (CTKD).
The structure holds PHY update event information.
Structure holds the data related to connection update event.
The structure represents the parameters of a remote connection parameter request event.
Structure holds the data of the remote features event.
Structure holds the LE device buffer indication event.
Structure representing the data for the length update event.
16 bit UUID format structure
32 bit UUID format structure
The Structure represents the error response event of GATT.
Structure representing a GATT descriptor event.
Structure representing the BLE event profiles list.
Structure to hold the BLE event profile by UUID.
Structure representing the BLE event for reading characteristic services by type.
Structure contains the service information received during the GATT read included services event.
Structure contains the service information received during the GATT read value by UUID event.
Structure representing the ATT value on GATT read response event.
The structure represents the set attribute response.
The structure represents the prepare write response.
The structure shows the list of received profiles. The maximum supported number of received profiles is 5.
The Structure represents the list of received profile descriptors of a particular profile. The maximum supported number of received profile descriptors is 5.
Structure to hold the response of characteristic services.
The structure represents the list of received included service attributes of a particular included service. The maximum supported number of received included service attributes is 5.
Structure represents the response for a Attribute Protocol (ATT) value.
Structure represents the list of received attribute descriptors. The maximum supported number of received attribute descriptors is 5.
Structure represents the add new service response.
Structure represents the response for local attribute value.
Structure represents the remote device information event.
Structure represents the received Remote Control Protocol (RCP) information event.
Structure indicates the received write information from the remote device.
Structure represents the GATT prepare write event.
Structure representing the BLE execute write request.
Structure representing the BLE read request.
Structure to hold the BLE MTU event information.
Structure to hold the MTU exchange information event.
Structure to hold the information of a directed advertising report event.
Structure representing the CBFC connection request event.
Structure representing the CBFC connection complete event.
Structure representing the CBFC received data event.
Structure representing the CBFC disconnection event.
ae adv report event
ae periodic sync establishment report event
ae periodic adv report event
ae periodic sync lost report event
ae scan timeout report event
ae adv set terminated report event
ae scan request recvd report event
Structure representing the BLE buffer statistics.
Callback function to be called when controller stats events are received from the module.
Functions#
Converts the given transmit power in dBm to power index.
Sends a connection request to a remote device using the Credit Based Flow Control (CBFC) mechanism.
Sends a connection response for a credit-based flow control (CBFC) connection.
Transmits data over a CBFC channel in the BLE module.
Disconnects a Connection-Based Flow Control (CBFC) connection with the specified device address and logical channel ID.
Typedef Documentation#
rsi_ble_event_adv_report_t#
typedef struct rsi_ble_event_adv_report_s rsi_ble_event_adv_report_t
Structure representing an advertising report event.
rsi_ble_event_conn_status_t#
typedef struct rsi_ble_event_conn_status_s rsi_ble_event_conn_status_t
Structure representing the connection status event in the module.
rsi_ble_event_enhance_conn_status_t#
typedef struct rsi_ble_event_enhnace_conn_status_s rsi_ble_event_enhance_conn_status_t
Structure representing the enhanced connection status event in the module.
rsi_ble_event_disconnect_t#
typedef struct rsi_ble_event_disconnect_s rsi_ble_event_disconnect_t
Disconnection event structure.
This structure contains information about the disconnection event.
rsi_ble_event_le_ping_time_expired_t#
typedef struct rsi_ble_event_le_ping_time_expired_s rsi_ble_event_le_ping_time_expired_t
The structure represents the LE ping timeout expired event.
rsi_bt_event_le_ltk_request_t#
typedef struct rsi_bt_event_le_ltk_request_s rsi_bt_event_le_ltk_request_t
The structure represents the Long Term Key (LTK) request event.
rsi_bt_event_le_security_keys_t#
typedef struct rsi_bt_event_le_security_keys_s rsi_bt_event_le_security_keys_t
The structure represents security keys event.
rsi_bt_event_encryption_enabled_t#
typedef struct rsi_bt_event_encryption_enabled_s rsi_bt_event_encryption_enabled_t
Structure to hold the event data for encryption enabled event.
rsi_bt_event_smp_req_t#
typedef struct rsi_bt_event_smp_req_s rsi_bt_event_smp_req_t
Structure to hold the Security Manager Protocol (SMP) request event.
rsi_bt_event_smp_resp_t#
typedef struct rsi_bt_event_smp_resp_s rsi_bt_event_smp_resp_t
Structure to hold the SMP response event data.
rsi_bt_event_smp_passkey_t#
typedef struct rsi_bt_event_smp_passkey_s rsi_bt_event_smp_passkey_t
Structure to hold the SMP passkey event data.
rsi_bt_event_smp_passkey_display_t#
typedef struct rsi_bt_event_smp_passkey_display_s rsi_bt_event_smp_passkey_display_t
Structure to hold the SMP passkey display event.
rsi_bt_event_sc_passkey_t#
typedef struct rsi_bt_event_sc_passkey_s rsi_bt_event_sc_passkey_t
Structure to hold the Secure Connections (SC) passkey event.
rsi_bt_event_smp_failed_t#
typedef struct rsi_bt_event_smp_failed_s rsi_bt_event_smp_failed_t
Structure to hold the information related to Security Manager Protocol (SMP) failed event.
rsi_bt_event_sc_method_t#
typedef struct rsi_bt_event_sc_method_s rsi_bt_event_sc_method_t
Structure to define the Bluetooth event security method.
rsi_ble_event_ctkd_t#
typedef struct rsi_bt_event_ctkd_s rsi_ble_event_ctkd_t
Structure representing the event for Cross Transport Key Derivation (CTKD).
This structure is used to define the parameters for the events related to CTKD, that includes the remote device address, and the derived key.
rsi_ble_event_phy_update_t#
typedef struct rsi_ble_event_phy_update_s rsi_ble_event_phy_update_t
The structure holds PHY update event information.
rsi_ble_event_conn_update_t#
typedef struct rsi_ble_event_conn_update_s rsi_ble_event_conn_update_t
Structure holds the data related to connection update event.
rsi_ble_event_remote_conn_param_req_t#
typedef struct rsi_ble_event_remote_conn_param_req_s rsi_ble_event_remote_conn_param_req_t
The structure represents the parameters of a remote connection parameter request event.
Note
The host does not receive a Connection Update callback event when the requested connection interval is the same as the current connection interval.
rsi_ble_event_remote_features_t#
typedef struct rsi_ble_event_remote_features_s rsi_ble_event_remote_features_t
Structure holds the data of the remote features event.
rsi_ble_event_le_dev_buf_ind_t#
typedef struct rsi_ble_event_le_dev_buf_ind_s rsi_ble_event_le_dev_buf_ind_t
Structure holds the LE device buffer indication event.
rsi_ble_event_data_length_update_t#
typedef struct rsi_ble_event_data_length_update_s rsi_ble_event_data_length_update_t
Structure representing the data for the length update event.
uuid128_t#
typedef struct uuid128_s uuid128_t
Structure representing a 128-bit Universal Unique IDentifier (UUID).
uuid_t#
typedef struct uuid_s uuid_t
Structure representing a Universally Unique Identifier (UUID).
This structure encapsulates a UUID, which can be of varying sizes— 16, 32, or 128-bits. It includes the size of the UUID, a reserved field, and a union to hold the value of one of the three types of UUIDs.
rsi_ble_event_error_resp_t#
typedef struct rsi_ble_event_error_resp_s rsi_ble_event_error_resp_t
The Structure represents the error response event of GATT.
rsi_ble_event_gatt_desc_t#
typedef struct rsi_ble_event_gatt_desc_s rsi_ble_event_gatt_desc_t
Structure representing a GATT descriptor event.
rsi_ble_event_profiles_list_t#
typedef struct rsi_ble_event_profiles_list_s rsi_ble_event_profiles_list_t
Structure representing the BLE event profiles list.
This structure is used to define the parameters for the BLE event profiles list, including the remote device address, number of profiles found, and the list of found profiles.
rsi_ble_event_profile_by_uuid_t#
typedef struct rsi_ble_event_profile_by_uuid_s rsi_ble_event_profile_by_uuid_t
Structure to hold the BLE event profile by UUID.
rsi_ble_event_read_by_type1_t#
typedef struct rsi_ble_event_read_by_type1_s rsi_ble_event_read_by_type1_t
Structure representing the BLE event for reading characteristic services by type.
This structure is used to represent the BLE event RSI_BLE_EVENT_GATT_READ_CHAR_SERVS with event ID 0x1503. It provides information related to the read operation of characteristic services.
rsi_ble_event_read_by_type2_t#
typedef struct rsi_ble_event_read_by_type2_s rsi_ble_event_read_by_type2_t
Structure contains the service information received during the GATT read included services event.
rsi_ble_event_read_by_type3_t#
typedef struct rsi_ble_event_read_by_type3_s rsi_ble_event_read_by_type3_t
Structure contains the service information received during the GATT read value by UUID event.
rsi_ble_event_att_value_t#
typedef struct rsi_ble_event_att_value_s rsi_ble_event_att_value_t
Structure representing the ATT value on GATT read response event.
rsi_ble_set_att_resp_t#
typedef struct rsi_ble_set_att_resp_s rsi_ble_set_att_resp_t
The structure represents the set attribute response.
rsi_ble_prepare_write_resp_t#
typedef struct rsi_ble_prepare_write_resp_s rsi_ble_prepare_write_resp_t
The structure represents the prepare write response.
rsi_ble_resp_profiles_list_t#
typedef struct rsi_ble_resp_profiles_list_s rsi_ble_resp_profiles_list_t
The structure shows the list of received profiles. The maximum supported number of received profiles is 5.
rsi_ble_resp_query_profile_descriptor_t#
typedef struct rsi_ble_resp_query_profile_descriptor_s rsi_ble_resp_query_profile_descriptor_t
The Structure represents the list of received profile descriptors of a particular profile. The maximum supported number of received profile descriptors is 5.
rsi_ble_resp_char_services_t#
typedef struct rsi_ble_resp_char_serv_s rsi_ble_resp_char_services_t
Structure to hold the response of characteristic services.
rsi_ble_resp_inc_services_t#
typedef struct rsi_ble_resp_inc_serv rsi_ble_resp_inc_services_t
The structure represents the list of received included service attributes of a particular included service. The maximum supported number of received included service attributes is 5.
rsi_ble_resp_att_value_t#
typedef struct rsi_ble_resp_att_value_s rsi_ble_resp_att_value_t
Structure represents the response for a Attribute Protocol (ATT) value.
rsi_ble_resp_att_descs_t#
typedef struct rsi_ble_resp_att_descs_s rsi_ble_resp_att_descs_t
Structure represents the list of received attribute descriptors. The maximum supported number of received attribute descriptors is 5.
rsi_ble_resp_add_serv_t#
typedef struct rsi_ble_resp_add_serv_s rsi_ble_resp_add_serv_t
Structure represents the add new service response.
rsi_ble_resp_local_att_value_t#
typedef struct rsi_ble_resp_local_att_value_s rsi_ble_resp_local_att_value_t
Structure represents the response for local attribute value.
rsi_ble_event_remote_device_info_t#
typedef struct rsi_ble_event_remote_device_info_s rsi_ble_event_remote_device_info_t
Structure represents the remote device information event.
This structure is used to define the parameters for a BLE event that provides information about a remote device.
rsi_ble_event_rcp_rcvd_info_t#
typedef struct rsi_ble_event_rcp_rcvd_info_s rsi_ble_event_rcp_rcvd_info_t
Structure represents the received Remote Control Protocol (RCP) information event.
This structure is used to define the parameters for a BLE event that involves receiving RCP information.
rsi_ble_event_write_t#
typedef struct rsi_ble_event_write_s rsi_ble_event_write_t
Structure indicates the received write information from the remote device.
rsi_ble_event_prepare_write_t#
typedef struct rsi_ble_event_prepare_write_s rsi_ble_event_prepare_write_t
Structure represents the GATT prepare write event.
rsi_ble_execute_write_t#
typedef struct rsi_ble_execute_write_s rsi_ble_execute_write_t
Structure representing the BLE execute write request.
This structure is used to define the parameters for an execute write request to a remote BLE device.
rsi_ble_read_req_t#
typedef struct rsi_ble_read_req_s rsi_ble_read_req_t
Structure representing the BLE read request.
This structure is used to define the parameters for a BLE read request, including the remote device address, attribute handle, request type, and offset.
rsi_ble_event_mtu_t#
typedef struct rsi_ble_event_mtu_s rsi_ble_event_mtu_t
Structure to hold the BLE MTU event information.
rsi_ble_event_mtu_exchange_information_t#
typedef struct rsi_ble_event_mtu_exchange_information_s rsi_ble_event_mtu_exchange_information_t
Structure to hold the MTU exchange information event.
rsi_ble_event_directedadv_report_t#
typedef struct rsi_ble_event_directedadv_report_s rsi_ble_event_directedadv_report_t
Structure to hold the information of a directed advertising report event.
rsi_ble_event_cbfc_conn_req_t#
typedef struct rsi_ble_event_cbfc_conn_req_s rsi_ble_event_cbfc_conn_req_t
Structure representing the CBFC connection request event.
This structure is used to define the parameters for a BLE event that involves a Circular Buffer Flow Control (CBFC) connection request from a remote device.
rsi_ble_event_cbfc_conn_complete_t#
typedef struct rsi_ble_event_cbfc_conn_complete_s rsi_ble_event_cbfc_conn_complete_t
Structure representing the CBFC connection complete event.
This structure is used to define the parameters for a BLE event that indicates the completion of a Circular Buffer Flow Control (CBFC) connection with a remote device.
rsi_ble_event_cbfc_rx_data_t#
typedef struct rsi_ble_event_cbfc_rx_data_s rsi_ble_event_cbfc_rx_data_t
Structure representing the CBFC received data event.
This structure is used to define the parameters for a BLE event that involves receiving data over a Circular Buffer Flow Control (CBFC) connection from a remote device.
rsi_ble_event_cbfc_disconn_t#
typedef struct rsi_ble_event_cbfc_disconn_s rsi_ble_event_cbfc_disconn_t
Structure representing the CBFC disconnection event.
This structure is used to define the parameters for a BLE event that involves the disconnection of a Circular Buffer Flow Control (CBFC) connection with a remote device.
rsi_ble_ae_adv_report_t#
typedef struct rsi_ble_ae_adv_report_s rsi_ble_ae_adv_report_t
ae adv report event
rsi_ble_per_adv_sync_estbl_t#
typedef struct rsi_ble_per_adv_sync_estbl_s rsi_ble_per_adv_sync_estbl_t
ae periodic sync establishment report event
rsi_ble_per_adv_report_t#
typedef struct rsi_ble_per_adv_report_s rsi_ble_per_adv_report_t
ae periodic adv report event
rsi_ble_per_adv_sync_lost_t#
typedef struct rsi_ble_per_adv_sync_lost_s rsi_ble_per_adv_sync_lost_t
ae periodic sync lost report event
rsi_ble_scan_timeout_t#
typedef struct rsi_ble_scan_timeout_s rsi_ble_scan_timeout_t
ae scan timeout report event
rsi_ble_adv_set_terminated_t#
typedef struct rsi_ble_adv_set_terminated_s rsi_ble_adv_set_terminated_t
ae adv set terminated report event
rsi_ble_scan_req_recvd_t#
typedef struct rsi_ble_scan_req_recvd_s rsi_ble_scan_req_recvd_t
ae scan request recvd report event
rsi_ble_event_enhance_conn_status_p#
typedef rsi_ble_event_enhance_conn_status_t* rsi_ble_event_enhance_conn_status_p
rsi_ble_event_data_length_update_p#
typedef rsi_ble_event_data_length_update_t* rsi_ble_event_data_length_update_p
rsi_ble_event_remote_conn_param_req_p#
typedef rsi_ble_event_remote_conn_param_req_t* rsi_ble_event_remote_conn_param_req_p
rsi_ble_event_remote_features_p#
typedef rsi_ble_event_remote_features_t* rsi_ble_event_remote_features_p
rsi_bt_event_encryption_enabled_p#
typedef rsi_bt_event_encryption_enabled_t* rsi_bt_event_encryption_enabled_p
rsi_bt_event_smp_passkey_display_p#
typedef rsi_bt_event_smp_passkey_display_t* rsi_bt_event_smp_passkey_display_p
rsi_bt_event_le_security_keys_p#
typedef rsi_bt_event_le_security_keys_t* rsi_bt_event_le_security_keys_p
rsi_ble_event_profile_by_uuid_p#
typedef rsi_ble_event_profile_by_uuid_t* rsi_ble_event_profile_by_uuid_p
rsi_ble_event_mtu_exchange_information_p#
typedef rsi_ble_event_mtu_exchange_information_t* rsi_ble_event_mtu_exchange_information_p
rsi_ble_event_le_dev_buf_ind_p#
typedef rsi_ble_event_le_dev_buf_ind_t* rsi_ble_event_le_dev_buf_ind_p
rsi_ble_event_set_buffer_config_p#
typedef rsi_ble_event_le_dev_buf_ind_t* rsi_ble_event_set_buffer_config_p
rsi_ble_event_indication_confirmation_p#
typedef rsi_ble_event_le_dev_buf_ind_t* rsi_ble_event_indication_confirmation_p
chip_ble_buffers_stats_t#
typedef struct chip_ble_buffers_stats_s chip_ble_buffers_stats_t
Structure representing the BLE buffer statistics.
This structure is used to define the parameters for BLE buffer statistics, including the utilization of Asynchronous Connection-Less (ACL) buffers and command packet buffers.
rsi_bt_event_controller_logs_t#
typedef struct rsi_bt_event_controller_logs_s rsi_bt_event_controller_logs_t
rsi_bt_on_controller_logs_t#
rsi_bt_on_controller_logs_t )(uint16_t resp_status, rsi_bt_event_controller_logs_t *controller_logs)
Callback function to be called when controller stats events are received from the module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | resp_statuscontains | the response status (Success or Error code) | |
| [in] | controller_logscontains | the controller stats parameters |
Returns
void
description#
This callback function will be called when controller stats events are received from the module. This callback has to be registered using rsi_bt_register_controller_stats_callbacks API.
Function Documentation#
rsi_convert_db_to_powindex#
uint8_t rsi_convert_db_to_powindex (int8_t tx_power_in_dBm)
Converts the given transmit power in dBm to power index.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int8_t | N/A | tx_power_in_dBm | The transmit power in dBm. |
This function takes a transmit power value in dBm and converts it to a power index value. The power index is used to set the transmit power level in the BLE module.
Returns
The power index corresponding to the given transmit power.
rsi_ble_cbfc_connreq#
uint32_t rsi_ble_cbfc_connreq (uint8_t * dev_addr, uint16_t psm)
Sends a connection request to a remote device using the Credit Based Flow Control (CBFC) mechanism.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | dev_addr | Pointer to the device address of the remote device. |
| uint16_t | N/A | psm | The Protocol Service Multiplexer (PSM) value. |
This function sends a connection request to a remote device using the CBFC mechanism. It takes the device address and the Protocol Service Multiplexer (PSM) as input parameters.
Returns
Returns a 32-bit unsigned integer indicating the status of the connection request.
0: If the connection request is successful.
Non-zero: If there is an error in sending the connection request.
rsi_ble_cbfc_connresp#
uint32_t rsi_ble_cbfc_connresp (uint8_t * dev_addr, uint16_t lcid, uint8_t result)
Sends a connection response for a credit-based flow control (CBFC) connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | dev_addr | The device address of the remote device. |
| uint16_t | N/A | lcid | The logical channel ID of the connection. |
| uint8_t | N/A | result | The result of the connection response. |
This function is used to send a connection response for a CBFC connection in the BLE module.
Returns
The status of the operation. Returns a 32-bit unsigned integer.
rsi_ble_cbfc_data_tx#
uint32_t rsi_ble_cbfc_data_tx (uint8_t * dev_addr, uint16_t lcid, uint16_t len, uint8_t * p_data)
Transmits data over a CBFC channel in the BLE module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | dev_addr | Pointer to the device address of the BLE module. |
| uint16_t | N/A | lcid | Logical channel ID of the CBFC channel. |
| uint16_t | N/A | len | Length of the data to be transmitted. |
| uint8_t * | N/A | p_data | Pointer to the data to be transmitted. |
This function is used to transmit data over a CBFC channel in the BLE module. It takes the device address, logical channel ID (LCID), length of the data, and a pointer to the data as input parameters. The function returns a 32-bit unsigned integer as the status of the transmission.
Returns
32-bit unsigned integer representing the status of the transmission.
rsi_ble_cbfc_disconnect#
uint32_t rsi_ble_cbfc_disconnect (uint8_t * dev_addr, uint16_t lcid)
Disconnects a Connection-Based Flow Control (CBFC) connection with the specified device address and logical channel ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | dev_addr | The device address of the remote device. |
| uint16_t | N/A | lcid | The logical channel ID of the CBFC connection. |
This function is used to disconnect a CBFC connection with the specified device address and logical channel ID.
Returns
The status code indicating the success or failure of the operation.
Returns 0 on success.
Returns a non-zero value on failure.