Structure holds the data of the remote features event.

Public Attributes#

uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_remote_features_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


remote_features#

uint8_t rsi_ble_event_remote_features_s::remote_features[RSI_BLE_REMOTE_FEATURES_LEN]

Remote device supported features

  • Note

    • Refer to spec for the supported features list.