Common#

Modules#

rsi_bt_resp_get_bt_stack_version_s

rsi_ble_set_antenna_s

rsi_bt_set_feature_bitmap_s

rsi_ble_oper_mode_s

rsi_ble_power_mode_s

rsi_bt_set_antenna_tx_power_level_s

rsi_bt_per_stats_s

rsi_bt_set_local_bd_addr_s

rsi_bt_cmd_update_gain_table_offset_or_maxpower_s

Typedefs#

Structure represents the Bluetooth response to get the BT stack version.

typedef struct rsi_ble_set_antenna_s

Structure represents the BLE set antenna request.

Structure represents the Bluetooth set feature bitmap.

typedef struct rsi_ble_oper_mode_s

Structure represents the BLE operation mode.

typedef struct rsi_ble_power_mode_s

Structure represents the BLE power mode.

Structure represents the Bluetooth set antenna transmit power level.

typedef struct rsi_bt_per_stats_s

Structure represents the Bluetooth Packet Error Rate (PER) statistics.

Structure represents the Bluetooth set local Bluetooth Device (BD) address.

Structure for updating gain table offset or max power in Bluetooth commands.

Functions#

int32_t
rsi_ble_set_ble_tx_power(int8_t tx_power)

Set TX power.

int32_t
rsi_bt_set_bd_addr(const uint8_t *dev_addr)

Set the device BD address. This is a blocking API.

int32_t
rsi_bt_set_local_name(const uint8_t *local_name)

Set the given name to local device. This is a blocking API.

int32_t
rsi_bt_cmd_update_gain_table_offset_or_max_pwr(uint8_t node_id, uint8_t payload_len, uint8_t *payload, uint8_t req_type)

Update gain table offset/max power. This is blocking API.

int32_t
rsi_bt_get_local_name(rsi_bt_resp_get_local_name_t *bt_resp_get_local_name)

Get the local device name. This is a blocking API.

int32_t
rsi_bt_get_rssi(uint8_t *dev_addr, int8_t *resp)

Get the RSSI of the remote device. This is a blocking API.

int32_t

Get the local device address. This is a blocking API.

int32_t
rsi_bt_get_bt_stack_version(rsi_bt_resp_get_bt_stack_version_t *bt_resp_get_bt_stack_version)

Get the BT stack version. This is a blocking API.

int32_t

Initialize the BT device. This is a blocking API.

int32_t

Deinitialize the BT device. This is a blocking API.

int32_t
rsi_bt_set_antenna(uint8_t antenna_value)

Select either internal / external antenna on the chip. This is a blocking API.

int32_t
rsi_bt_power_save_profile(uint8_t psp_mode, uint8_t psp_type)

Select the power save profile mode for BT / BLE. This is a blocking API.

int32_t
rsi_bt_per_stats(uint8_t cmd_type, struct rsi_bt_per_stats_s *per_stats)

Request the local device for BT PER operation.

Typedef Documentation#

rsi_bt_resp_get_bt_stack_version_t#

typedef struct rsi_bt_resp_get_bt_stack_version_s rsi_bt_resp_get_bt_stack_version_t

Structure represents the Bluetooth response to get the BT stack version.

This structure is used to define the parameters for the response that includes the Bluetooth stack version.


rsi_ble_set_antenna_t#

typedef struct rsi_ble_set_antenna_s rsi_ble_set_antenna_t

Structure represents the BLE set antenna request.

This structure is used to define the parameters for setting the BLE antenna, that includes the antenna value which, can be internal or external.


rsi_bt_set_feature_bitmap_t#

typedef struct rsi_bt_set_feature_bitmap_s rsi_bt_set_feature_bitmap_t

Structure represents the Bluetooth set feature bitmap.

This structure is used to define the parameters for setting the Bluetooth feature bitmap, which includes feature bits in a bit map format.


rsi_ble_oper_mode_t#

typedef struct rsi_ble_oper_mode_s rsi_ble_oper_mode_t

Structure represents the BLE operation mode.

This structure is used to define the parameters for the BLE operation mode, that includes Bluetooth features, and the module type.


rsi_ble_power_mode_t#

typedef struct rsi_ble_power_mode_s rsi_ble_power_mode_t

Structure represents the BLE power mode.

This structure is used to define the parameters for setting the BLE power mode, that includes the power mode and Ultra-Low-Power (ULP) mode enable settings.


rsi_bt_set_antenna_tx_power_level_t#

typedef struct rsi_bt_set_antenna_tx_power_level_s rsi_bt_set_antenna_tx_power_level_t

Structure represents the Bluetooth set antenna transmit power level.

This structure is used to define the parameters for setting the antenna transmit power level, which includes the protocol mode and transmit power.


rsi_bt_per_stats_t#

typedef struct rsi_bt_per_stats_s rsi_bt_per_stats_t

Structure represents the Bluetooth Packet Error Rate (PER) statistics.

This structure is used to define the parameters for collecting Bluetooth PER statistics, that includes counts of CRC fails, successful transmissions, and other relevant metrics.


rsi_bt_set_local_bd_addr_t#

typedef struct rsi_bt_set_local_bd_addr_s rsi_bt_set_local_bd_addr_t

Structure represents the Bluetooth set local Bluetooth Device (BD) address.

This structure is used to define the parameters for setting the local Bluetooth device address.


rsi_bt_cmd_update_gain_table_offset_or_maxpower_t#

typedef struct rsi_bt_cmd_update_gain_table_offset_or_maxpower_s rsi_bt_cmd_update_gain_table_offset_or_maxpower_t

Structure for updating gain table offset or max power in Bluetooth commands.


Function Documentation#

rsi_ble_set_ble_tx_power#

int32_t rsi_ble_set_ble_tx_power (int8_t tx_power)

Set TX power.

Parameters
TypeDirectionArgument NameDescription
int8_t[in]tx_power

Power value

Returns

  • The following values are returned:

    • 0 - Success

    • Non-zero value - Failure

    • 0x4E02 - Unknown connection identifier

    • 0x4E01 - Unknown HCI command

    • 0x4E0C - Command disallowed

    • 0x4046 - Invalid arguments

    • 0x4D04 - BLE not connected

    • 0x4D14 - BLE parameter out of mandatory range This is a Blocking API. Refer to the Status Codes section for the above error codes at wiseconnect-status-codes.

Note

  • The higher power will be backed off based on country region. For SiW917Y1GA and SiW917Y1GN module boards, region configuration is not supported. These boards always use the world_safe region. Hence, the maximum TX power is limited by the world_safe regulatory limits. When the DUT is connected in AP mode, the output power is the minimum of the host transmit power and the maximum power allowed for the country region. When it is not connected to an AP, the maximum output power is world_safe. This API currently supports controlling the TX power in the configured chain during wireless initialization. However, changing the chain from LP to HP or vice versa is not supported. Use the following setting to indicate tx_power as an index: #define RSI_BLE_PWR_INX 30 Default value for power index is 31. Valid values for power index range from 1 to 31 and 33 to 127:

    • 1 to 31 : BLE - 0 dBm mode.

    • 33 to 63 : BLE - 10 dBm mode.

    • 64 to 82 : BLE - 1 dBm - 18 dBm HP mode in the resolution of 1 dBm.

    • 104 to 126: BLE - 0.5 dBm - 11 dBm HP mode in the resolution of 0.5 dBm.

    • 127 : BLE HP Mode, maximum power supported.

  • Use the following setting to indicate tx_power in dBm (-8 to 18 dBm): #define RSI_BLE_PWR_INX_DBM 1

  • For the LP Chain - Power index vs output power in dBm in E2E mode:

    Power Index

    Output Power in dBm

    1

    -22.3054959

    2

    -16.59332574

    3

    -13.38278365

    4

    -11.19804718

    5

    -9.576522466

    6

    -8.312070432

    7

    -7.294640362

    8

    -6.458448154

    9

    -5.760963318

    10

    -5.173042366

    11

    -4.673788189

    12

    -4.247653993

    13

    -3.882708784

    14

    -3.569545894

    15

    -3.300567503

    16

    -3.069499167

    17

    -2.871050592

    18

    -2.700672503

    19

    -2.554378603

    20

    -2.428612817

    21

    -2.32014891

    22

    -2.226013876

    23

    -2.143429275

    24

    -2.069766557

    25

    -2.002513642

    26

    -1.939250859

    27

    -1.87763493

    28

    -1.815390046

    29

    -1.750305305

    30

    -1.680237892

    31

    -1.603121401

    32

    N/A

    33

    -10.4822997

    34

    -4.9531679

    35

    -1.931961022

    36

    0.057132993

    37

    1.476764101

    38

    2.5332116

    39

    3.336771823

    40

    3.953605265

    41

    4.426779615

    42

    4.786171523

    43

    5.053647759

    44

    5.246007208

    45

    5.37676618

    46

    5.457304255

    47

    5.497635316

    48

    5.506945838

    49

    5.493978354

    50

    5.467302132

    51

    5.435491631

    52

    5.407220119

    53

    5.391268248

    54

    5.396444507

    55

    5.431416481

    56

    5.504458826

    57

    5.62313521

    58

    5.793945208

    59

    6.02197959

    60

    6.310634089

    61

    6.661428559

    62

    7.073964236

    63

    7.546029076

  • For the HP Chain - Power index vs output power in dBm in E2E mode:

    Power Index

    Output Power in dBm

    64

    1

    65

    2

    66

    3

    67

    4

    68

    5

    69

    6

    70

    7

    71

    8

    72

    9

    73

    10

    74

    11

    75

    12

    76

    13

    77

    14

    78

    15

    -

    -

    -

    -

    104

    0.5

    105

    1

    106

    1.5

    107

    2

    108

    2.5

    109

    3

    110

    3.5

    111

    4

    -

    -

    126

    10.5

    127

    Max Power Supported by Country region


rsi_bt_set_bd_addr#

int32_t rsi_bt_set_bd_addr (const uint8_t * dev_addr)

Set the device BD address. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]dev_addr

- Public address of the device to be set.

  • Pre-conditions:

    • Needs to be called immediately after device initialization.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

    • 3 - Command is given in wrong state (that is, not immediate after opermode)

Note


rsi_bt_set_local_name#

int32_t rsi_bt_set_local_name (const uint8_t * local_name)

Set the given name to local device. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]local_name

- Name to be set to the local device.

  • Pre-conditions:

    • Device should be initialized before calling this API.

Note

  • For BLE alone Opermode : When the name of the local device is set to a value with length more than 16 bytes then error is returned with an error code 0x4E66.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_cmd_update_gain_table_offset_or_max_pwr#

int32_t rsi_bt_cmd_update_gain_table_offset_or_max_pwr (uint8_t node_id, uint8_t payload_len, uint8_t * payload, uint8_t req_type)

Update gain table offset/max power. This is blocking API.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]node_id

- Node ID (0 - BLE, 1 - BT).

uint8_t[in]payload_len

- Length of the payload.

uint8_t *[in]payload

- Payload containing table data of gain table offset/max power

uint8_t[in]req_type

- Update gain table request type

  • 0 - Max power update.

  • 1 - Max power offset update.

  • 2 - LP_Chain 0 dBm offset update.

  • 3 - LP_chain 10 dBm offset update.

  • Pre-conditions:

    • Device should be initialized before calling this API.

Returns

  • The following values are returned:

    • 0 - Success.

    • 0x4F01 - Invalid gain table payload length.

    • 0x4F02 - Invalid region.

    • 0x4F03 - Invalid gain table offset request type.

    • 0x4F04 - Invalid node id.

Note


rsi_bt_get_local_name#

int32_t rsi_bt_get_local_name (rsi_bt_resp_get_local_name_t * bt_resp_get_local_name)

Get the local device name. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
rsi_bt_resp_get_local_name_t *[out]bt_resp_get_local_name

- This parameter is the response buffer to hold the response of this API. Refer to rsi_bt_resp_get_local_name_s structure for more information.

  • Pre-conditions:

    • Device should be initialized before calling this API.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_get_rssi#

int32_t rsi_bt_get_rssi (uint8_t * dev_addr, int8_t * resp)

Get the RSSI of the remote device. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[in]dev_addr

- Remote device address.

int8_t *[out]resp

- Parameter to hold the response of this API, RSSI is filled in this resp parameter.

  • Pre-conditions:

    • rsi_bt_connect() API need to be called before this API.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_get_local_device_address#

int32_t rsi_bt_get_local_device_address (uint8_t * resp)

Get the local device address. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]resp

- Parameter to hold the response of this API, local bd_addr is filled in this resp parameter.

  • Pre-conditions:

    • Device should be initialized before calling this API.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_get_bt_stack_version#

int32_t rsi_bt_get_bt_stack_version (rsi_bt_resp_get_bt_stack_version_t * bt_resp_get_bt_stack_version)

Get the BT stack version. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
rsi_bt_resp_get_bt_stack_version_t *[out]bt_resp_get_bt_stack_version

- Response buffer to hold the response of this API. Refer to rsi_bt_resp_get_bt_stack_version_s structure for more info

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_init#

int32_t rsi_bt_init (void )

Initialize the BT device. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
voidN/A
  • Pre-conditions:

    • Device should be initialized before calling this API.

    • If the device is in powersave, get back the device to ACTIVE MODE by using rsi_bt_power_save_profile()

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_deinit#

int32_t rsi_bt_deinit (void )

Deinitialize the BT device. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
voidN/A
  • Pre-conditions:

    • Device should be initialized before this API.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_set_antenna#

int32_t rsi_bt_set_antenna (uint8_t antenna_value)

Select either internal / external antenna on the chip. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]antenna_value

- Parameter is used to select either internal or external antenna. Possible values:

  • 0x00 RSI_SEL_INTERNAL_ANTENNA

  • 0x01 RSI_SEL_EXTERNAL_ANTENNA

  • Pre-conditions:

    • Device should be initialized before calling this API.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note


rsi_bt_power_save_profile#

int32_t rsi_bt_power_save_profile (uint8_t psp_mode, uint8_t psp_type)

Select the power save profile mode for BT / BLE. This is a blocking API.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]psp_mode

Following psp_mode is defined.

  • 0 - RSI_ACTIVE. In this mode module is active and power save is disabled.

  • 1 - RSI_SLEEP_MODE_1. On mode. In this sleep mode, SoC would never turn off, therefore no handshake is required before sending data to the module. BT/BLE does not support this mode.

  • 2 - RSI_SLEEP_MODE_2. Connected sleep mode. In this sleep mode, SoC will go to sleep based on GPIO or Message, therefore handshake is required before sending data to the module.

  • 8 - RSI_SLEEP_MODE_8 :Deep sleep mode with RAM RETENTION.

  • 10- RSI_SLEEP_MODE_10 : Deep sleep mode without RAM RETENTION. In this sleep mode, module would turn off the SoC. Since SoC is turn off, therefore handshake is required before sending data to the module.

uint8_t[in]psp_type

Following psp_type is defined.

  • 0 - RSI_MAX_PSP. This psp_type would be used for max power saving.

  • 1 - Fast PSP.

  • Pre-conditions:

    • Device should be initialized before calling this API

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note

  • If the user wants to enable power save in CoEx mode (WLAN + BT LE) mode - It is mandatory to enable WLAN power save along with BT LE power save.

  • The device will enter into power save if and only if both protocol (WLAN, BLE) power save modes are enabled.

  • Refer to the Status Codes section for the above error codes at wiseconnect-status-codes.

  • psp_type is only valid in psp_mode 2.

    • BT/BLE does not support in RSI_SLEEP_MODE_1.

    • BT/BLE supports only RSI_MAX_PSP mode. Remaining modes are not supported.


rsi_bt_per_stats#

int32_t rsi_bt_per_stats (uint8_t cmd_type, struct rsi_bt_per_stats_s * rsi_bt_per_stats)

Request the local device for BT PER operation.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]cmd_type

- Parameter to define the command id type as per operation.

  • BT_PER_STATS_CMD_ID (0x08) - Command id enables as per statistics.

  • BT_TRANSMIT_CMD_ID (0x15) - Command id enables as per transmit.

  • BT_RECEIVE_CMD_ID (0x16) - Command id enables as per receive.

struct rsi_bt_per_stats_s *[in]rsi_bt_per_stats

- reference to the response structure. Refer to rsi_bt_per_stats_s structure for more information.

  • Pre-conditions:

    • Call rsi_bt_per_tx() or rsi_bt_per_rx() before calling this API.

Returns

  • The following values are returned:

    • 0 - Success

    • Non-Zero Value - Failure

Note

  • Refer to Error Codes section for common error codes.