The structure represents the parameters of a remote connection parameter request event.

Note

  • The host does not receive a Connection Update callback event when the requested connection interval is the same as the current connection interval.

Public Attributes#

uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_remote_conn_param_req_s::dev_addr[RSI_DEV_ADDR_LEN]

Device address of the remote device


conn_interval_min#

uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_min

Minimum connection interval


conn_interval_max#

uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_max

Maximum connection interval


conn_latency#

uint16_t rsi_ble_event_remote_conn_param_req_s::conn_latency

Slave Latency


timeout#

uint16_t rsi_ble_event_remote_conn_param_req_s::timeout

Supervision Timeout