Power Manager#
Introduction#
The Power Manager is a platform-level software module that manages the system's power states. The power state requirements are set by the different software modules (drivers, stacks, application code, etc...). Power Manager also offers a notification mechanism through which any piece of software module can be notified of power state transitions through callbacks.
Initialization
Power Manager must be initialized before any call to the Power Manager API. If sl_system is used, only sl_system_init() must be called, otherwise sl_si91x_power_manager_init() must be called manually.
Power Manager Architecture


Add and remove requirements
The driver/application can add and remove power state requirements at runtime. Adding requirement function calls changes the power state. Removing requirement function calls will not have any effect for state transition. sl_si91x_power_manager_add_peripheral_requirement()
sl_si91x_power_manager_remove_peripheral_requirement()
Subscribe to events
It is possible to get notified when the system transitions from a power state to another power state. This can allow to do some operations depending on which level the system goes, such as saving/restoring context. sl_si91x_power_manager_subscribe_ps_transition_event()
sl_si91x_power_manager_unsubscribe_ps_transition_event()
Memory Footprint Analysis
Memory footprint analysis helps in understanding the memory usage of the application.
It includes details about stack, heap, and global/static memory usage.
Tools like map files or IDE-specific memory analyzers can be used to analyze the memory footprint.
Optimizing memory usage ensures efficient resource utilization and avoids memory overflows.
In this example, ensure that the stack size (3072 bytes) and other memory allocations are sufficient for the application's requirements.
Tickless idle Mode
Application Task: This represents tasks running in your application. These tasks might call vTaskDelay or other blocking functions, leading the scheduler to consider them idle.
Scheduler (Idle): When no tasks are ready to run, the scheduler enters an idle state.
Check for Idle: The scheduler checks if FreeRTOS tickless mode is enabled (configUSE_TICKLESS_IDLE=1) and if all tasks are blocked.
Suspend Ticks & Enter Sleep: If conditions are met, the scheduler calls vPortSuppressTicksAndSleep to:
Disable the system tick interrupt.
start a timer to track the sleep duration.
Enter a low-power mode using MCU power management features (e.g., Wait For Interrupt instruction).
Wakeup Interrupt: An interrupt (event or timer) wakes up the MCU.
Scheduler Update: The scheduler calculates the sleep duration and adjusts the system tick counter accordingly.
Resume Scheduler & Tasks: The scheduler resumes the tick interrupt and exits the low-power mode. Tasks become ready to run again.
Application Code: Application tasks continue execution based on the updated system time.


Sleep
When the software has no more operations and only needs to wait for an event, the software must call sl_si91x_power_manager_sleep().
Query callback functions
Is OK to sleep
Between the time sl_si91x_power_manager_sleep() is called and the MCU goes to sleep, an ISR may occur and require the system to resume at that time instead of sleeping. In this case, a callback is called in a critical section to validate that the MCU can go to sleep.
The function sl_si91x_power_manager_is_ok_to_sleep() will be generated automatically by Simplicity Studio's wizard. The function will look at multiple software modules from the SDK to make a decision. The application can contribute to the decision by defining the function app_is_ok_to_sleep(). If any of the software modules (including the application via app_is_ok_to_sleep()) return false, the process of entering in sleep will be aborted.
Sleep on ISR exit
When the system enters sleep, the only way to wake it up is via an interrupt or exception. By default, Power Manager will assume that when an interrupt occurs and the corresponding ISR has been executed, the system must not go back to sleep. However, in the case where all the processing related to this interrupt is performed in the ISR, it is possible to go back to sleep by using this hook.
The function sl_si91x_power_manager_sleep_on_isr_exit() will be generated automatically by Simplicity Studio's wizard. The function will look at multiple software modules from the SDK to make a decision. The application can contribute to the decision by defining the function app_sleep_on_isr_exit(). The generated function will make a decision based on the value returned by the different software modules (including the application via app_sleep_on_isr_exit()):
SL_SI91X_POWER_MANAGER_ISR_IGNORE: if the software module did not cause the system wakeup and/or doesn't want to contribute to the decision.
SL_SI91X_POWER_MANAGER_ISR_SLEEP: if the software module did cause the system wakeup, but the system should go back to sleep.
SL_SI91X_POWER_MANAGER_ISR_WAKEUP: if the software module did cause the system wakeup, and the system should not go back to sleep.
If any software module returned SL_SI91X_POWER_MANAGER_ISR_SLEEP and none returned SL_SI91X_POWER_MANAGER_ISR_WAKEUP, the system will go back to sleep. Any other combination will cause the system not to go back to sleep.


Debugging feature
By installing the Power Manager debug component and setting the configuration define SL_SI91X_POWER_MANAGER_DEBUG to 1, it is possible to record the requirements currently set and their owner. It is possible to print a table at any time that lists all the added requirements and their owner. This table can be printed by calling the function: Make sure to add the following define
#define CURRENT_MODULE_NAME // Module printable name here
to any application code source file that adds and removes requirements.
Configuration#
Power Manager allows configuration of RAM retention, peripheral states, wakeup sources, and clock scaling.
Clock Scaling:
Clock can be configured as power-save or performance based on the user requirement. By default after the state change, the clock is configured as powersave. The below API is used to set the clock scaling. sl_si91x_power_manager_set_clock_scaling(); where mode can be either power-save or performance.
Peripheral States:
High power, ULPSS, and NPSS peripherals can be configured using the below APIs. They can be powered on or off based on user requirements. sl_si91x_power_manager_add_peripheral_requirement()sl_si91x_power_manager_remove_peripheral_requirement();
RAM retention:
Retains the RAM in low power state either by using size or RAM bank as input parameter. sl_si91x_power_manager_configure_ram_retention();
Wakeup source:
The wakeup sources can be configured using the below API. sl_si91x_power_manager_set_wakeup_sources();
Usage#
Initialization:
sl_si91x_power_manager_init(): Initializes the Power Manager service and sets the initial power state.
Peripheral requirements:
sl_si91x_power_manager_add_peripheral_requirement(): Turns on/off the peripheral power
sl_si91x_power_manager_remove_peripheral_requirement(): Removes the peripheral requirement.
Power State Transitions:
sl_si91x_power_manager_subscribe_ps_transition_event(): Registers a callback for a specific power state transition.
sl_si91x_power_manager_sleep(): To Put the device into sleep mode.
sl_si91x_power_manager_unsubscribe_ps_transition_event(): Unregisters the callback for the power state transition.
De-initialization:
sl_si91x_power_manager_deinit(): De-initializes the Power Manager service.
Usage Example
#define PS_EVENT_MASK ( SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS4\
| SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_LEAVING_PS4 \
| SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS3\
| SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_LEAVING_PS3 \
| SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS2\
| SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_LEAVING_PS2 \
| SL_SI91X_POWER_MANAGER_EVENT_TRANSITION_LEAVING_SLEEP)
static void power_manager_app(void)
{
sl_status_t status;
sl_power_manager_ps_transition_event_handle_t handle;
sl_power_manager_ps_transition_event_info_t info = { .event_mask = PS_EVENT_MASK, .on_event = transition_callback };
// Subscribe the state transition callback events, the ored value of flag and function pointer is passed in this API.
status = sl_si91x_power_manager_subscribe_ps_transition_event(&handle, &info);
if (status != SL_STATUS_OK) {
// If status is not OK, return with the error code.
return;
}
// Configuring the RAM retention used for sleep-wakeup.
sl_power_ram_retention_config_t config;
config.configure_ram_banks = true;
config.m4ss_ram_banks = SL_SI91X_POWER_MANAGER_M4SS_RAM_BANK_8 | SL_SI91X_POWER_MANAGER_M4SS_RAM_BANK_9 | SL_SI91X_POWER_MANAGER_M4SS_RAM_BANK_10;
config.ulpss_ram_banks = SL_SI91X_POWER_MANAGER_ULPSS_RAM_BANK_2 | SL_SI91X_POWER_MANAGER_ULPSS_RAM_BANK_3;
// RAM retention modes are configured and passed into this API.
status = sl_si91x_power_manager_configure_ram_retention(&config);
if (status != SL_STATUS_OK) {
// If status is not OK, return with the error code.
return;
}
// Change state to PS2
sl_si91x_power_manager_add_ps_requirement(SL_SI91X_POWER_MANAGER_PS2);
// CODE BLOCK //
// Change state to PS4
// Removed PS2 requirement as it is no longer required.
sl_si91x_power_manager_remove_ps_requirement(SL_SI91X_POWER_MANAGER_PS2);
sl_si91x_power_manager_add_ps_requirement(SL_SI91X_POWER_MANAGER_PS2);
// SLEEP_WAKEUP
// Initialize wakeup source
// Replace the wakeup source peripheral macro defined in sl_si91x_power_manager.h file
// It sets the below peripheral as wakeup source
sl_si91x_power_manager_set_wakeup_sources(WAKEUP_SOURCE, true);
sl_si91x_power_manager_sleep();
}
Modules#
sl_power_ram_retention_config_t
sl_power_manager_ps_transition_event_info_t
sl_power_manager_ps_transition_event_handle_t
Enumerations#
Enumeration for the power states.
Enumeration for clock scaling parameters.
On ISR Exit Hook answer.
Typedefs#
Type for storing IRQ state during critical sections (PRIMASK).
Mask of all the event(s) to listen to.
Typedef for the user-supplied callback function which is called when a power state transition occurs.
Functions#
To initialize the Power Manager service.
To disable the interrupts.
To enable the interrupts.
To add a requirement on power states.
To remove requirement on power states.
To configure the clock scaling.
the clock scaling mode in PS4 and PS3 power state.
Adds the peripheral requirement.
To remove the peripheral requirement.
To register a callback to be called on given power state transition(s).
To unregister an event callback handle on power state transition.
To move into sleep mode and wait for the peripheral to be set as a wakeup source to trigger and wake up the M4 SoC.
To move into standby state and wait for the interrupt.
To configure the wakeup sources.
To retain the RAM in low power state either by using size or RAM bank as input parameters.
To return the current power state.
To get the current requirements on all the power states.
Requests the PS1 state requirement during tickless idle mode.
Remove the PS1 state request during tickless idle mode.
Get the current ps1 state request status from the power manager during tickless idle mode.
Requests the standby state during tickless idle mode.
Remove the standby state request during tickless idle mode.
Get the current standby state request status during tickless idle mode.
Check if a TX command is currently in progress.
To de-initialize the Power Manager service.
Performs pre-transition checks before entering PS2 state.
To print a table that describes the current requirements on each power state and their owner.
Macros#
sl power manager event transition for entering PS4 state.
sl power manager event transition for leaving PS4 state.
sl power manager event transition for entering PS3 state.
sl power manager event transition for leaving PS3 state.
sl power manager event transition for entering PS2 state.
sl power manager event transition for leaving PS2 state.
sl power manager event transition for leaving PS1 state.
sl power manager event transition for leaving sleep state.
Event transition for leaving standby state.
Deep Sleep Timer based wakeup source.
Wireless based wakeup source.
GPIO based wakeup source.
Comparator based wakeup source.
Sysrtc based wakeup source.
ULP peripheral based wakeup source.
SDC (Sensor data collector) based wakeup source.
Alarm based wakeup source.
Second based wakeup source.
Milli second based wakeup source.
Watchdog interrupt based wakeup source.
M4SS EFUSE Power Gate.
M4SS RPDMA Power Gate.
M4SS SDIO SPI Power Gate.
M4SS QSPI and ICACHE Power Gate.
M4SS IID Power Gate.
M4SS M4 Debug Power Gate.
M4SS M4 Core Power Gate.
M4SS External ROM Power Gate.
ULP Miscellaneous Power Gate.
DEPRECATED - ULP Capacitive Touch Sensor Power Gate.
ULP UART Power Gate.
ULP SSI Power Gate.
ULP I2S Power Gate.
ULP I2C Power Gate.
ULP AUX Power Gate.
ULP IR Power Gate.
ULP UDMA Power Gate.
ULP FIM Power Gate.
NPSS MCU BFFS (Battery FF's) Power Gate.
NPSS MCU FSM Power Gate.
NPSS MCU RTC (Real Time Clock) Power Gate.
NPSS MCU WDT (Watchdog Timer) Power Gate.
NPSS MCU Process Sensor Power Gate.
NPSS MCU Temperature Sensor Power Gate.
NPSS MCU Storage 1 Power Gate.
NPSS MCU Storage 2 Power Gate.
NPSS MCU Storage 3 Power Gate.
NPSS Time Period Power Gate.
NPSS MCU APB Control Power Gate.
4 KB (Bank 1 of first 192k chunk)
4 KB (Bank 2 of first 192k chunk)
4 KB (Bank 3 of first 192k chunk)
4 KB (Bank 4 of first 192k chunk)
4 KB (Bank 5 of first 192k chunk)
32 KB (Bank 6-7 of first 192k chunk)
64 KB (Bank 9-11 of first 192k chunk)
64 KB (Bank 12-15 of first 192k chunk)
64 KB (Bank 1-4 of second 192k chunk)
64 KB (Bank 1-4 of third 192k chunk)
2 KB
2 KB
2 KB
2 KB
Enumeration Documentation#
sl_power_state_t#
sl_power_state_t
Enumeration for the power states.
| Enumerator | |
|---|---|
| SL_SI91X_POWER_MANAGER_PS0 | PS0 Power State. |
| SL_SI91X_POWER_MANAGER_PS1 | PS1 Power State. |
| SL_SI91X_POWER_MANAGER_PS2 | PS2 Power State. |
| SL_SI91X_POWER_MANAGER_PS3 | PS3 Power State. |
| SL_SI91X_POWER_MANAGER_PS4 | PS4 Power State. |
| SL_SI91X_POWER_MANAGER_SLEEP | Sleep. |
| SL_SI91X_POWER_MANAGER_STANDBY | Standby. |
| LAST_ENUM_POWER_STATE | Last enum for validation. |
sl_clock_scaling_t#
sl_clock_scaling_t
Enumeration for clock scaling parameters.
| Enumerator | |
|---|---|
| SL_SI91X_POWER_MANAGER_POWERSAVE | Minimum supported frequency in a power state. |
| SL_SI91X_POWER_MANAGER_PERFORMANCE | Maximum supported frequency in a power state. |
| LAST_ENUM_CLOCK_SCALING | Last enum for validation. |
sl_si91x_power_manager_on_isr_exit_t#
sl_si91x_power_manager_on_isr_exit_t
On ISR Exit Hook answer.
| Enumerator | |
|---|---|
| SL_SI91X_POWER_MANAGER_ISR_IGNORE | The module did not trigger an ISR and it does not want to contribute to the decision. |
| SL_SI91X_POWER_MANAGER_ISR_SLEEP | The module was the one that caused the system wakeup and the system SHOULD go back to sleep. |
| SL_SI91X_POWER_MANAGER_ISR_WAKEUP | The module was the one that caused the system wakeup and the system MUST NOT go back to sleep. |
Typedef Documentation#
sli_si91x_power_manager_irq_state_t#
typedef uint32_t sli_si91x_power_manager_irq_state_t
Type for storing IRQ state during critical sections (PRIMASK).
sl_power_manager_ps_transition_event_t#
typedef uint32_t sl_power_manager_ps_transition_event_t
Mask of all the event(s) to listen to.
sl_power_manager_ps_transition_on_event_t#
typedef void(* sl_power_manager_ps_transition_on_event_t) (sl_power_state_t from, sl_power_state_t to) )(sl_power_state_t from, sl_power_state_t to)
Typedef for the user-supplied callback function which is called when a power state transition occurs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | from | Power state we are leaving. | |
| N/A | to | Power state we are entering. |
This typedef defines a callback function that is called when a power state transition occurs.
Function Documentation#
sl_si91x_power_manager_init#
sl_status_t sl_si91x_power_manager_init (void )
To initialize the Power Manager service.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The application is configured to start in the PS3 Powersave state with a clock frequency of 40MHz.
Note
The Power Manager initialization is automatically handled within the sl_service_init() function. Users do not need to manually initialize the Power Manager, ensuring a hassle-free setup process.
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_ALREADY_INITIALIZED - Power Manager is already initialized.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_core_entercritical#
__STATIC_INLINE void sl_si91x_power_manager_core_entercritical (void )
To disable the interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This API is deprecated.
Disables all interrupts by setting PRIMASK. Fault exception handlers will still be enabled.
sl_si91x_power_manager_core_exitcritical#
__STATIC_INLINE void sl_si91x_power_manager_core_exitcritical (void )
To enable the interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This API is deprecated.
Enables interrupts by clearing PRIMASK.
sl_si91x_power_manager_add_ps_requirement#
__STATIC_INLINE sl_status_t sl_si91x_power_manager_add_ps_requirement (sl_power_state_t state)
To add a requirement on power states.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_state_t | [in] | state | Power state to add requirement: sl_power_state_t
|
The default state for the Power Manager is PS3. The maximum number of requirements that can be added is 255. The Power Manager switches to the state if it is a valid transition. Before transitioning from one state to another, make sure to remove requirements of previous states if any were added. If an invalid state requirement is added, it returns SL_STATUS_INVALID_PARAMETER. If the Power Manager service is not initialized, it returns SL_STATUS_NOT_INITIALIZED. To initialize, call sl_si91x_power_manager_init. To get the requirements on all power states, call sl_si91x_power_manager_get_requirement_table. To know the current power state, use sl_si91x_power_manager_get_current_state.
Pre-conditions:
sl_si91x_power_manager_ps2_pre_check (if PS2 state is added along with WiFi component)
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
Note
Critical section pairing: on failure,
SLI_SI91X_POWER_MANAGER_CORE_EXIT_CRITICAL()runs for every state except when adding PS1 (legacy behavior). On success, EXIT runs for all states except PS1; for PS1, EXIT happens insidesli_si91x_power_manager_change_power_state_with_critical_irq()beforetrigger_sleepso interrupts are enabled for waking up from retention sleep (seesli_si91x_power_manager_core_exitcritical()). WithSL_SI91X_TICKLESS_MODE1,cpsiei is enabled fromvPortSuppressTicksAndSleep; otherwise, PS2 to PS1 may still issuecpsiei after wake up whenirq_statewas0at entry.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_remove_ps_requirement#
__STATIC_INLINE sl_status_t sl_si91x_power_manager_remove_ps_requirement (sl_power_state_t state)
To remove requirement on power states.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_state_t | [in] | state | Power state to remove requirement: sl_power_state_t
|
Default state for Power Manager is PS3. Requirements added to a power state must be removed in pairs to ensure proper state transitions. If a requirement is added for a specific power state (e.g., PS4) and not removed, the application will be unable to transition to a lower power state. For instance, if a requirement on PS4 is added but not removed, the Power Manager will remain in PS4 and cannot transition to a lower power state.
Note
: If the current state is PS4 and no other requirements are added, removing the PS4 requirement will cause the device to remain in its last active state, which in this case is PS4.
Pre-conditions:
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - The Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_set_clock_scaling#
sl_status_t sl_si91x_power_manager_set_clock_scaling (sl_clock_scaling_t mode)
To configure the clock scaling.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_clock_scaling_t | [in] | mode | Clock scaling mode (of type sl_clock_scaling_t). |
PS4 and PS3 states are supported only. Possible values for clock scaling are:
POWERSAVE and PERFORMANCE
PS4 Performance: 180 MHz clock
PS4 Power-save: 100 MHz clock
PS3 Performance: 80 MHz clock
PS3 Power-save: 40 MHz clock
For PS2 state, 20 MHz clock is default.
If the Power Manager service is not initialized, it returns SL_STATUS_NOT_INITIALIZED. To initialize, call sl_si91x_power_manager_init.
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
SL_STATUS_INVALID_CONFIGURATION - Invalid configuration of mode.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_get_clock_scaling#
sl_clock_scaling_t sl_si91x_power_manager_get_clock_scaling (void )
the clock scaling mode in PS4 and PS3 power state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Possible return values: * SL_SI91X_POWER_MANAGER_POWERSAVE (Minimum supported frequency in a power state) SL_SI91X_POWER_MANAGER_PERFORMANCE (Maximum supported frequency in a power state)
Returns
The following values are returned:
sl_clock_scaling_t enum value indicating current clock scaling mode
sl_si91x_power_manager_add_peripheral_requirement#
sl_status_t sl_si91x_power_manager_add_peripheral_requirement (sl_power_peripheral_t * peripheral)
Adds the peripheral requirement.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_peripheral_t * | [in] | peripheral | Structure for different peripherals sl_power_peripheral_t. |
Power on the peripherals the valid peripherals passed in the structure. Structure member possible values: sl_power_peripheral_t
m4ss_peripheral -> Accepts masked value of m4ss peripherals.
ulpss_peripheral -> Accepts masked value of ulpss peripherals.
npss_peripheral -> Accepts masked value of npss peripherals. The values of enums can be combined by using 'OR' operator and then passed to the variable.
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_INVALID_STATE (0x0002) - Not a valid transition.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
Note
The user must take care of the initialization of the peripherals added.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_remove_peripheral_requirement#
sl_status_t sl_si91x_power_manager_remove_peripheral_requirement (sl_power_peripheral_t * peripheral)
To remove the peripheral requirement.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_peripheral_t * | [in] | peripheral | Structure for different peripherals sl_power_peripheral_t. |
Powers off the peripherals specified in the structure. Valid peripherals are passed in the structure sl_power_peripheral_t. The structure members can have the following values:
m4ss_peripheral -> Accepts masked value of M4SS peripherals.
ulpss_peripheral -> Accepts masked value of ULPSS peripherals.
npss_peripheral -> Accepts masked value of NPSS peripherals.
The values of enums can be combined using the 'OR' operator and then passed to the variable.
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_subscribe_ps_transition_event#
sl_status_t sl_si91x_power_manager_subscribe_ps_transition_event (sl_power_manager_ps_transition_event_handle_t * event_handle, const sl_power_manager_ps_transition_event_info_t * event_info)
To register a callback to be called on given power state transition(s).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_manager_ps_transition_event_handle_t * | [in] | event_handle | Event handle (no initialization needed). |
| const sl_power_manager_ps_transition_event_info_t * | [in] | event_info | Event info structure that contains the event mask and the callback that must be called. |
If the Power Manager service is not initialized, it returns SL_STATUS_NOT_INITIALIZED. To initialize, call sl_si91x_power_manager_init.
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_NULL_POINTER - Null pointer is passed.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
Note
Adding and removing power state transition requirement(s) from a callback on a transition event is not supported.
The parameters passed must be persistent, meaning that they need to survive until the callback fires.
An ASSERT is thrown if the handle is not found.
Usage example:
#define PS_EVENT_MASK ( SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS4 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_PS4 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS3 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_PS3 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS2 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_PS2 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_PS0 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_SLEEP)
sl_power_manager_ps_transition_event_handle_t handle;
sl_power_manager_ps_transition_event_info_t info = { .event_mask = PS_EVENT_MASK,
.on_event = transition_callback };
void transition_callback(sl_power_state_t from, sl_power_state_t to)
{
[...]
}
void main(void)
{
sl_status_t status;
status = sl_si91x_power_manager_init();
// Validate the status
status = sl_si91x_power_manager_subscribe_ps_transition_event(&handle, &info);
// Validate the status
}
sl_si91x_power_manager_unsubscribe_ps_transition_event#
sl_status_t sl_si91x_power_manager_unsubscribe_ps_transition_event (sl_power_manager_ps_transition_event_handle_t * event_handle, const sl_power_manager_ps_transition_event_info_t * event_info)
To unregister an event callback handle on power state transition.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_manager_ps_transition_event_handle_t * | [in] | event_handle | Event handle which must be unregistered (must have been registered previously). |
| const sl_power_manager_ps_transition_event_info_t * | [in] | event_info | Event info structure that contains the event mask and the callback that must be called. |
If the Power Manager service is not initialized, it returns SL_STATUS_NOT_INITIALIZED. To initialize, call sl_si91x_power_manager_init.
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_NULL_POINTER - Null pointer is passed.
For more information on status codes, refer to SL STATUS DOCUMENTATION. Note
An ASSERT is thrown if the handle is not found.
sl_si91x_power_manager_sleep#
sl_status_t sl_si91x_power_manager_sleep (void )
To move into sleep mode and wait for the peripheral to be set as a wakeup source to trigger and wake up the M4 SoC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
It supports PS4, PS3, and PS2 only; it cannot enter sleep mode from any other active states. If any error occurs, it returns the error code and does not transition to sleep mode.
Note
This function expects and calls a callback with the following signature:
boolean_t sl_si91x_power_manager_is_ok_to_sleep(void). This function can be used to cancel a sleep action and handle the possible race condition where an ISR that would cause a wakeup is triggered right after the decision to call sl_si91x_power_manager_sleep() has been made.
This function also expects and calls a callback with the following signature: boolean_t sl_si91x_power_manager_isr_wakeup(void) after wakeup from sleep. The possible return values are:
SL_SI91X_POWER_MANAGER_ISR_IGNORE
SL_SI91X_POWER_MANAGER_ISR_SLEEP
SL_SI91X_POWER_MANAGER_ISR_WAKEUP
Note
It can end up in an infinite sleep-wakeup loop if continuously SL_SI91X_POWER_MANAGER_ISR_SLEEP return value is passed.
Pre-conditions:
sl_si91x_power_manager_init
sl_si91x_power_manager_configure_ram_retention
sl_si91x_power_manager_set_wakeup_sources
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
SL_STATUS_INVALID_STATE (0x0002) - Not a valid transition.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_standby#
void sl_si91x_power_manager_standby (void )
To move into standby state and wait for the interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Standby transition is possible from PS4, PS3, and PS2 states only. Transition from sleep, PS1, or PS0 is not supported.
Note
Applications using RTOS with tickless mode enabled must not call this API. This API is not supposed to be used directly in the application and is called automatically when the system is in an idle state with tickless mode.
Pre-conditions:
sl_si91x_power_manager_set_wakeup_sources#
sl_status_t sl_si91x_power_manager_set_wakeup_sources (uint32_t source, boolean_t add)
To configure the wakeup sources.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | source | (uint32_t) Wakeup sources. |
| boolean_t | [in] | add | (boolean_t) True enables and false disables the wakeup source. |
Once the wakeup source is set by the Universal Configurator (UC), the Power Manager automatically handles the initialization, User need to install the appropriate wakeup component based on the configured wakeup source.
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_INVALID_PARAMETER - Invalid parameter is passed.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_configure_ram_retention#
sl_status_t sl_si91x_power_manager_configure_ram_retention (sl_power_ram_retention_config_t * config)
To retain the RAM in low power state either by using size or RAM bank as input parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_ram_retention_config_t * | [in] | config | Structure for the parameters of RAM retention sl_power_ram_retention_config_t. |
Structure member possible values: sl_power_ram_retention_config_t
configure_ram_banks -> Boolean to switch between RAM Bank retentions. Either by size or by RAM bank number.
Enable -> Use RAM Bank Number.
Disable -> Use Size.
m4ss_ram_size_kb -> Retains M4SS RAM banks according to the size.
Less than 320 KB (Enter 100 for 100 KB).
ulpss_ram_size_kb -> Retains ULPSS RAM banks according to the size.
Less than 8 KB (Enter 5 for 5 KB).
ram_bank_number -> Retains the M4SS and ULPSS RAM Bank using bank number.
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_NOT_INITIALIZED - Power Manager is not initialized.
SL_STATUS_NULL_POINTER - Null pointer is passed.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_power_manager_get_current_state#
sl_power_state_t sl_si91x_power_manager_get_current_state (void )
To return the current power state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Possible return values:
2: SL_POWER_MANAGER_PS2, ///< PS2 Power State
3: SL_POWER_MANAGER_PS3, ///< PS3 Power State
4: SL_POWER_MANAGER_PS4, ///< PS4 Power State
Returns
sl_power_state_t enum value indicating the current power state.
sl_si91x_power_manager_get_requirement_table#
uint8_t * sl_si91x_power_manager_get_requirement_table (void )
To get the current requirements on all the power states.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
It returns 5 values starting from PS0 to PS4.
Pre-conditions:
Returns
Pointer to a uint8_t type array which contains 5 elements.
Usage example:
void main()
{
uint8_t *requirement_table;
sl_si91x_power_manager_init();
requirement_table = sl_si91x_power_manager_get_requirement_table();
DEBUGOUT("PS4: %d, PS3: %d, PS2: %d, PS1: %d, PS0: %d",
requirement_table[4],
requirement_table[3],
requirement_table[2],
requirement_table[1],
requirement_table[0]);
}
Retrieve the power state requirement table for the power manager.
This function provides access to the power state requirement table, which is used to manage and track the power state requirements of various components or modules in the system. The table contains information about the power states or dependencies required by different modules.
Note
The returned pointer points to a table managed internally by the power manager. Ensure that the table is not modified directly to avoid unexpected behavior.
Returns
Pointer to the power state requirement table.
This API can be used to query the current power state requirements of the system and make decisions based on the power states of various components. For example, it can be used in scenarios where power optimization or power state transitions are required.
sl_si91x_power_manager_request_ps1_state#
sl_status_t sl_si91x_power_manager_request_ps1_state (void )
Requests the PS1 state requirement during tickless idle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function requests the PS1 power state from the power manager during tickless idle mode. If the system is in the IDLE state, it transitions into the PS1 state.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - PS1 state requirement successfully added.
SL_STATUS_INVALID_STATE (0x0002) - Invalid request to add PS1 state.
SL_STATUS_NOT_INITIALIZED (0x0011) - Power manager service is not initialized.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
sl_si91x_power_manager_remove_ps1_state_request#
sl_status_t sl_si91x_power_manager_remove_ps1_state_request (void )
Remove the PS1 state request during tickless idle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function removes the PS1 state request from the power manager during tickless idle mode.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Ps1 state requirement successfully removed.
SL_STATUS_INVALID_STATE (0x0002) - Invalid request to remove PS1 state.
SL_STATUS_NOT_INITIALIZED (0x0011) - Power manager service is not initialized.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
sl_si91x_power_manager_get_ps1_state_status#
bool sl_si91x_power_manager_get_ps1_state_status (void )
Get the current ps1 state request status from the power manager during tickless idle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function indicates whether a PS1 state request has been added to the power manager during tickless idle mode.
Returns
Status code indicating the result:
true - PS1 state requirement is added.
false - PS1 state requirement is not added.
sl_si91x_power_manager_request_standby_state#
sl_status_t sl_si91x_power_manager_request_standby_state (void )
Requests the standby state during tickless idle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function requests the standby power state from the power manager during tickless idle mode. If the system is in the IDLE state, it transitions into the standby state.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Standby state requirement successfully added.
SL_STATUS_INVALID_STATE (0x0002) - Invalid request to add standby state.
sl_si91x_power_manager_remove_standby_state_request#
sl_status_t sl_si91x_power_manager_remove_standby_state_request (void )
Remove the standby state request during tickless idle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function removes the standby state request from the power manager during tickless idle mode.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) : Standby state requirement successfully removed.
SL_STATUS_INVALID_STATE (0x0002) - Invalid request to remove standby state.
sl_si91x_power_manager_get_standby_state_status#
bool sl_si91x_power_manager_get_standby_state_status (void )
Get the current standby state request status during tickless idle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function indicates whether a standby state request has been added to the power manager during tickless idle mode.
Returns
Status code indicating the result:
true : Standby state requirement is added.
false : Standby state requirement is not added.
sl_si91x_power_manager_is_tx_command_in_progress#
bool sl_si91x_power_manager_is_tx_command_in_progress (void )
Check if a TX command is currently in progress.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function is used to check the TX command status. It returns true if a TX command is currently in progress; otherwise, it returns false otherwise.
Pre-conditions:
The Wi-Fi component must be added to the project for this function to work properly. If it is not included, this function will always return false.
Returns
bool - Returns true if TX command is in progress; otherwise, returns false otherwise.
Note
This function is useful for power management decisions and determining when the system is ready for sleep or other power state transitions.
sl_si91x_power_manager_deinit#
void sl_si91x_power_manager_deinit (void )
To de-initialize the Power Manager service.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
It clears all the power requirements and callback event subscriptions. If the Power Manager service is not initialized, it returns SL_STATUS_NOT_INITIALIZED. To initialize, call sl_si91x_power_manager_init.
Pre-conditions:
sl_si91x_power_manager_ps2_pre_check#
bool sl_si91x_power_manager_ps2_pre_check (void )
Performs pre-transition checks before entering PS2 state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function verifies whether the Network Wireless Processor (NWP) has any pending packet transfers to the M4 core. If pending packets are detected, it returns false to prevent PS2 state transition and avoid data loss. Wi-Fi component must be included in the project for this function to operate correctly.
Returns
Status code indicating the result:
true - Safe to enter PS2 state (no pending packets).
false - Pending packets detected, PS2 transition should be blocked.
sl_si91x_power_manager_debug_print_ps_requirements#
void sl_si91x_power_manager_debug_print_ps_requirements (void )
To print a table that describes the current requirements on each power state and their owner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |