Structure to store configuration parameters for RAM retention.
Public Attributes#
uint16_t
M4SS RAM size that needs to be restored.
uint16_t
ULPSS RAM size that needs to be restored.
boolean_t
Enable will set the RAM banks using size, disable sets RAM banks using bank number.
uint32_t
M4SS RAM bank number that needs to be restored.
uint32_t
ULPSS RAM bank number that needs to be restored.
Public Attribute Documentation#
m4ss_ram_size_kb#
uint16_t sl_power_ram_retention_config_t::m4ss_ram_size_kb
M4SS RAM size that needs to be restored.
ulpss_ram_size_kb#
uint16_t sl_power_ram_retention_config_t::ulpss_ram_size_kb
ULPSS RAM size that needs to be restored.
configure_ram_banks#
boolean_t sl_power_ram_retention_config_t::configure_ram_banks
Enable will set the RAM banks using size, disable sets RAM banks using bank number.
m4ss_ram_banks#
uint32_t sl_power_ram_retention_config_t::m4ss_ram_banks
M4SS RAM bank number that needs to be restored.
ulpss_ram_banks#
uint32_t sl_power_ram_retention_config_t::ulpss_ram_banks
ULPSS RAM bank number that needs to be restored.