Access Point#
Functions#
Start a Wi-Fi access point (AP) interface.
Reconfigure the dynamic parameters of a Wi-Fi Access point (AP) interface.
Get the configuration of a Wi-Fi AP interface.
Set the advanced configuration options of a running Wi-Fi access point (AP).
Get the advanced configuration options of a running Wi-Fi access point interface.
Stop Wi-Fi access point.
Disconnects a client with the specified MAC address from Access Point (AP).
Return the Wi-Fi client information of all clients connected to the AP.
Return a list of Wi-Fi clients connected to the Wi-Fi access point.
Provide the number of Wi-Fi clients connected to the Wi-Fi access point.
Function Documentation#
sl_wifi_start_ap#
sl_status_t sl_wifi_start_ap (sl_wifi_interface_t interface, const sl_wifi_ap_configuration_t * configuration)
Start a Wi-Fi access point (AP) interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| const sl_wifi_ap_configuration_t * | [in] | configuration | Wi-Fi AP configuration. See sl_wifi_ap_configuration_t |
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
For AP mode with WPA3 security, only SAE-H2E method is supported. SAE hunting and pecking method is not supported. TKIP encryption mode is not supported. Encryption mode is automatically configured to CCMP. PMKSA is not supported in WPA3 AP mode.
Management Frame Protection (MFP) behavior in AP mode:
For WPA2 security: MFP is NOT automatically enabled. Use sl_wifi_set_mfp before calling this API if MFP is required.
For WPA3 security: MFP is automatically enabled as required by the WPA3 standard.
In FCC-certified modules,Region configuration is not supported and if triggered returns error SL_STATUS_SI91X_FEATURE_NOT_AVAILABLE.
AP supports only 1 to 11 channels.
AP does not advertise the Country IE.
sl_wifi_reconfigure_ap#
sl_status_t sl_wifi_reconfigure_ap (sl_wifi_interface_t interface, sl_wifi_ap_reconfiguration_t config)
Reconfigure the dynamic parameters of a Wi-Fi Access point (AP) interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| sl_wifi_ap_reconfiguration_t | [in] | config | Wi-Fi AP dynamic configuration. See sl_wifi_ap_reconfiguration_t |
sl_wifi_start_ap should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
The access point continues to transmit beacons when a client is connected, regardless of the beacon_stop configuration.
sl_wifi_get_ap_configuration#
sl_status_t sl_wifi_get_ap_configuration (sl_wifi_interface_t interface, sl_wifi_ap_configuration_t * configuration)
Get the configuration of a Wi-Fi AP interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| sl_wifi_ap_configuration_t * | [out] | configuration | sl_wifi_ap_configuration_t object that contains the AP configuration. |
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
sl_wifi_set_advanced_ap_configuration#
sl_status_t sl_wifi_set_advanced_ap_configuration (sl_wifi_interface_t interface, const sl_wifi_advanced_ap_configuration_t * configuration)
Set the advanced configuration options of a running Wi-Fi access point (AP).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| const sl_wifi_advanced_ap_configuration_t * | [in] | configuration | Wi-Fi AP advanced configuration. See sl_wifi_advanced_ap_configuration_t |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API is not yet implemented.
sl_wifi_get_advanced_ap_configuration#
sl_status_t sl_wifi_get_advanced_ap_configuration (sl_wifi_interface_t interface, const sl_wifi_advanced_ap_configuration_t * configuration)
Get the advanced configuration options of a running Wi-Fi access point interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| const sl_wifi_advanced_ap_configuration_t * | [out] | configuration | sl_wifi_advanced_ap_configuration_t object that will contain the AP advanced configuration. |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API is not yet implemented.
sl_wifi_stop_ap#
sl_status_t sl_wifi_stop_ap (sl_wifi_interface_t interface)
Stop Wi-Fi access point.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi Access Point interface as identified by sl_wifi_interface_t |
Pre-conditions:
sl_wifi_start_ap should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
All si91x, BSD, and IoT sockets associated with the AP interface must be closed before invoking this API.
sl_wifi_disconnect_ap_client#
sl_status_t sl_wifi_disconnect_ap_client (sl_wifi_interface_t interface, const sl_mac_address_t * mac, sl_wifi_deauth_reason_t reason)
Disconnects a client with the specified MAC address from Access Point (AP).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi Access Point interface as identified by sl_wifi_interface_t |
| const sl_mac_address_t * | [in] | mac | Wi-Fi client's MAC address of type sl_mac_address_t |
| sl_wifi_deauth_reason_t | [in] | reason | Reason for de-authentication as specified in sl_wifi_deauth_reason_t |
Use this function to disassociate (disconnect) a client from Access Point. This API is used when the device is in AP mode.
Pre-conditions:
sl_wifi_start_ap should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API is supported only in AP mode.
sl_wifi_get_ap_client_info#
sl_status_t sl_wifi_get_ap_client_info (sl_wifi_interface_t interface, sl_wifi_client_info_response_t * client_info)
Return the Wi-Fi client information of all clients connected to the AP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi Access Point interface as identified by sl_wifi_interface_t |
| sl_wifi_client_info_response_t * | [out] | client_info | sl_wifi_client_info_response_t object to store the client info. |
Pre-conditions:
sl_wifi_start_ap should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API is supported only in AP mode.
sl_wifi_get_ap_client_list#
sl_status_t sl_wifi_get_ap_client_list (sl_wifi_interface_t interface, uint16_t client_list_count, sl_mac_address_t * client_list)
Return a list of Wi-Fi clients connected to the Wi-Fi access point.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi Access Point interface as identified by sl_wifi_interface_t |
| uint16_t | [in] | client_list_count | The number of sl_mac_address_t objects the client_list can store. |
| sl_mac_address_t * | [out] | client_list | A pointer to an array of client_list_count number of sl_mac_address_t objects where the client list will be copied to. |
Pre-conditions:
sl_wifi_start_ap should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API is supported only in AP mode.
sl_wifi_get_ap_client_count#
sl_status_t sl_wifi_get_ap_client_count (sl_wifi_interface_t interface, uint32_t * client_count)
Provide the number of Wi-Fi clients connected to the Wi-Fi access point.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi Access Point interface as identified by sl_wifi_interface_t |
| uint32_t * | [out] | client_count | A uint32_t pointer that will store the number of associated clients. |
Pre-conditions:
sl_wifi_start_ap should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API is supported only in AP mode.