Wi-Fi Access Point configuration structure.

Indicates the configuration parameters for setting up a Wi-Fi Access Point (AP).

Note

  • When configuring AP interface in open security mode, the credential ID must be set to SL_WIFI_NO_CREDENTIAL_ID.

  • The security field refers to the security type of the Wi-Fi AP. In Wi-Fi access-point mode, the AP supports OPEN, WPA-PSK, WPA2-PSK, WPA/WPA2 Mixed, and WPA3 security modes. Valid configurations are:

    • SL_WIFI_OPEN - For OPEN security mode (no encryption)

    • SL_WIFI_WPA - For WPA-PSK security mode

    • SL_WIFI_WPA2 - For WPA2-PSK security mode

    • SL_WIFI_WPA_WPA2_MIXED - For WPA/WPA2 mixed security mode

    • SL_WIFI_WPA3 - For WPA3 security mode

  • client_idle_timeout - This is the period after which the AP will disconnect the station if there are no wireless exchanges from the station to the AP. The keep-alive period is calculated in terms of 32 multiples of the beacon interval (i.e, if there are no wireless transfers from station to AP within a (32 x beacon_interval) time units (where 1 TU = 1024 microseconds) time period, the station will be disconnected). If null data-based method is selected, the AP checks the connectivity of the station by sending null data packet. If the station does not acknowledge the packet, that station will be disconnected from the AP after 4 retries. The maximum valid range supported is up to 255.

Public Attributes#

SSID (Service Set Identifier) of the Access Point.

Security mode of the Access Point.

Encryption mode of the Access Point.

Channel configuration of the Access Point.

Rate protocol of the Access Point.

Optional flags for AP configuration.

ID of secure credentials.

uint8_t

Keep alive type of the access point. One of the values from sl_wifi_ap_keepalive_type_t

uint16_t

Beacon interval of the access point in time units (1 TU = 1024 microseconds)

uint32_t

Period after which AP will disconnect the station.

uint16_t

Number of beacons per DTIM.

uint8_t

The maximum number of associated clients must not exceed SL_WIFI_CUSTOM_FEAT_MAX_NUM_OF_CLIENTS. If this bit is not set in device configuration, the default maximum is 8 clients in AP-only mode and 4 clients in concurrent mode.

uint8_t

Flag to stop beaconing when there are no associated clients.

Flags to enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.

uint8_t

A flag to enable 11n.

Public Attribute Documentation#

ssid#

sl_wifi_ssid_t sl_wifi_ap_configuration_t::ssid

SSID (Service Set Identifier) of the Access Point.


security#

sl_wifi_security_t sl_wifi_ap_configuration_t::security

Security mode of the Access Point.


encryption#

sl_wifi_encryption_t sl_wifi_ap_configuration_t::encryption

Encryption mode of the Access Point.


channel#

sl_wifi_channel_t sl_wifi_ap_configuration_t::channel

Channel configuration of the Access Point.


rate_protocol#

sl_wifi_rate_protocol_t sl_wifi_ap_configuration_t::rate_protocol

Rate protocol of the Access Point.


options#

sl_wifi_ap_flag_t sl_wifi_ap_configuration_t::options

Optional flags for AP configuration.

Note

  • Dynamic configurability of hidden SSIDs is only available in APCONF when it is disabled in opermode.


credential_id#

sl_wifi_credential_id_t sl_wifi_ap_configuration_t::credential_id

ID of secure credentials.


keepalive_type#

uint8_t sl_wifi_ap_configuration_t::keepalive_type

Keep alive type of the access point. One of the values from sl_wifi_ap_keepalive_type_t


beacon_interval#

uint16_t sl_wifi_ap_configuration_t::beacon_interval

Beacon interval of the access point in time units (1 TU = 1024 microseconds)


client_idle_timeout#

uint32_t sl_wifi_ap_configuration_t::client_idle_timeout

Period after which AP will disconnect the station.


dtim_beacon_count#

uint16_t sl_wifi_ap_configuration_t::dtim_beacon_count

Number of beacons per DTIM.


maximum_clients#

uint8_t sl_wifi_ap_configuration_t::maximum_clients

The maximum number of associated clients must not exceed SL_WIFI_CUSTOM_FEAT_MAX_NUM_OF_CLIENTS. If this bit is not set in device configuration, the default maximum is 8 clients in AP-only mode and 4 clients in concurrent mode.


beacon_stop#

uint8_t sl_wifi_ap_configuration_t::beacon_stop

Flag to stop beaconing when there are no associated clients.


tdi_flags#

sl_wifi_tdi_t sl_wifi_ap_configuration_t::tdi_flags

Flags to enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.


is_11n_enabled#

uint8_t sl_wifi_ap_configuration_t::is_11n_enabled

A flag to enable 11n.