Wi-Fi Listen interval structure.
Specifies the Wi-Fi Listen interval in time units (1 TU = 1024 microseconds). The listen interval is the time interval between two consecutive Target Beacon Transmission (TBTT) events. Moving forward, this structure will be deprecated. Instead, use the sl_wifi_listen_interval_v2_t structure. This is retained for backward compatibility.
Public Attributes#
uint32_t
Wi-Fi Listen interval in time units (1 TU = 1024 microseconds)