Wi-Fi Operational Statistics structure.

Public Attributes#

uint8_t

Operating mode of the Wi-Fi interface.

uint8_t

DTIM (Delivery Traffic Indication Message) period. Indicates the number of beacon intervals between DTIM frames.

uint8_t

Ideal beacon information.

uint8_t

Busy beacon information.

uint8_t

Beacon interval. Indicates the time interval between successive beacons, in Time Units (TUs).

Public Attribute Documentation#

operating_mode#

uint8_t sl_wifi_operational_statistics_t::operating_mode

Operating mode of the Wi-Fi interface.


dtim_period#

uint8_t sl_wifi_operational_statistics_t::dtim_period

DTIM (Delivery Traffic Indication Message) period. Indicates the number of beacon intervals between DTIM frames.


ideal_beacon_info#

uint8_t sl_wifi_operational_statistics_t::ideal_beacon_info[SL_WIFI_OPERATIONAL_STATISTICS_FIELD_UINT16_OCTETS]

Ideal beacon information.


busy_beacon_info#

uint8_t sl_wifi_operational_statistics_t::busy_beacon_info[SL_WIFI_OPERATIONAL_STATISTICS_FIELD_UINT16_OCTETS]

Busy beacon information.


beacon_interval#

uint8_t sl_wifi_operational_statistics_t::beacon_interval[SL_WIFI_OPERATIONAL_STATISTICS_FIELD_UINT16_OCTETS]

Beacon interval. Indicates the time interval between successive beacons, in Time Units (TUs).