Channel bitmap for scanning in a set of selective channels.
Note
A 2.4 GHz channel is enabled by setting the bit of the corresponding channel number minus 1. For example, for channel 1, set bit 0; for channel 2, set bit 1, and so on. sl_wifi_scan_configuration_t
5 GHz chnannels are not supported in SiWx91x devices.
Public Attributes#
uint16_t
Channel bitmap for scanning in a set of selective channels in 2.4 GHz.
uint32_t
Channel bitmap for scanning in a set of selective channels in 5 GHz. (Not supported in SiWx91x devices).
Public Attribute Documentation#
channel_bitmap_2_4#
uint16_t sl_wifi_channel_bitmap_t::channel_bitmap_2_4
Channel bitmap for scanning in a set of selective channels in 2.4 GHz.
channel_bitmap_5#
uint32_t sl_wifi_channel_bitmap_t::channel_bitmap_5
Channel bitmap for scanning in a set of selective channels in 5 GHz. (Not supported in SiWx91x devices).