SiWx91x Power Manager AT Commands#

Commands#

wifisys-wake-src#

Configures the wakeup source (from sleep) for the application processor of the SiWx91x device.

Command Format#

at+wifisys-wake-src=<source>,<add>

Related SDK API#

sl_si91x_configure_wakeup_sources

Pre-conditions#

  • A peripheral designated as the wakeup source (for example, Calendar) should be configured before sending this command.

    • A Calendar or ULP Timer wakeup source is usually configured before sending this command and started after sending this command.

    • See the Calendar AT commands for starting an alarm with the Calendar peripheral.

Parameters#

source#

A numeric value specifying the wakeup source.

add#

Set to 1 or 0 to add or remove the wakeup source indicated in the source parameter.

Response#

Notes#

  • Wakeup Sources. Currently supporting only SL_SI91X_POWER_MANAGER_ALARM_WAKEUP source.

Examples#

at+wifisys-wake-src=0x4000000,1         # Add the wakeup source

wifisys-psreq#

Configures the power state requirements of the application processor of the SiWx91x device.

Command Format#

at+wifisys-psreq=<state>,<add>

Related SDK APIs#

Pre-conditions#

Parameters#

state#

The power state requirement to be added or removed. Contains a numeric value that corresponds to one of the sl_power_state_t enum values.

add#

Set to 1 or 0 to add or remove the requirement indicated in the state parameter.

Response#

sl_si91x_power_manager_init, sl_si91x_power_manager_add_ps_requirement, or sl_si91x_power_manager_get_requirement_table API.

Notes#

  • If the Power Manager service on the SiWx91x device is not already initialized, it will be initialized first by invoking the sl_si91x_power_manager_init API.

  • If add is set to 1, the sl_si91x_power_manager_add_ps_requirement API is invoked; otherwise, sl_si91x_power_manager_remove_ps_requirement is invoked.

  • The SiWx91x application processor will immediately transition to the specified power state if it is valid and add is set to 1.

Examples#

at+wifisys-psreq=0,1        # Transition to the PS0 power state

wifisys-psreq?#

Queries the current power state requirements of the application processor of the SiWx91x device.

Command Format#

at+wifisys-psreq?

Related SDK API#

sl_si91x_power_manager_get_requirement_table

Pre-conditions#

Parameters#

None

Response#

  • OK <ps0> <ps1> <ps2> <ps3> <ps4> in case of success, where <psN> is an integer value specifying the requirements for the corresponding power state.

  • ERROR <error code> in case of error. Possible error codes are the same as those returned by the sl_si91x_power_manager_get_requirement_table API.

Notes#

If the Power Manager service on the SiWx91x device is not already initialized, it will be initialized first by invoking the sl_si91x_power_manager_init API.

Examples#

at+wifisys-psreq?
OK 1 0 0 0 0   

wifisys-ps?#

Queries the current power state of the application processor of the SiWx91x device.

Command Format#

at+wifisys-ps?

Related SDK API#

sl_si91x_power_manager_get_current_state

Pre-conditions#

Parameters#

None

Response#

  • OK <state> in case of success, where <state> is the current power state (for example, PS0) of the SiWx91x device, populated with a numeric value corresponding to one of the values of the enum sl_power_state_t.

  • ERROR <error code> in case of error. Possible error codes are the same as those returned by the sl_si91x_power_manager_get_current_state API.

Notes#

  • If the Power Manager service on the SiWx91x device is not already initialized, it will be initialized first by invoking the sl_si91x_power_manager_init API.

Examples#

at+wifisys-ps?
OK 0  

wifisys-sleep#

Places the SiWx91x device into a sleep state where it waits for a wakeup source.

Command Format#

at+wifisys-sleep

Related SDK API#

Note: sl_si91x_power_manager_sleep is deprecated in WiSeConnect SDK v4.1.0. Prefer the Power Manager service and tickless idle integration for new applications. See Migrating from v4.0.2.

sl_si91x_power_manager_sleep

Pre-conditions#

Parameters#

None

Response#

  • OK in case of success,

  • ERROR <error code> in case of error. Possible error codes are the same as those returned by the sl_si91x_power_manager_sleep API.

Notes#

  • If the Power Manager service on the SiWx91x device is not already initialized, it will be initialized first by invoking the sl_si91x_power_manager_init API.

Examples#

at+wifisys-sleep 

wifisys-standby#

Places the SiWx91x device into a standby state, where it awaits an interrupt. This low-power mode preserves the device's context, enabling a rapid wake-up in response to external events or interrupts. While in standby, the system retains essential state information and significantly reduces power consumption compared to active operation.

Command Format#

at+wifisys-standby

Related SDK API#

sl_si91x_power_manager_standby

Pre-conditions#

Parameters#

None

Note#

  • If the Power Manager service on the SiWx91x device is not already initialized, it will be initialized first by invoking the sl_si91x_power_manager_init API.

Response#

Examples#

at+wifisys-standby

Events#

WIFISYS_PS_TRANSITION#

Event message sent by the SiWx91x device when a transition occurs between two power states.

Event Message Format#

at+WIFISYS_PS_TRANSITION=<from-state>,<to-state>

Related SDK API#

Callback type sl_power_manager_ps_transition_on_event_t

Parameters#

from-state#

The previous power state that the SiWx91x device has moved out of. Contains a numeric value that corresponds to one of the values of the enum sl_power_state_t. See the sl_power_state_t documentation for possible values.

to-state#

The current power state that the SiWx91x device has moved into. Contains a numeric value that corresponds to one of the values of the enum sl_power_state_t.

Examples#

at+WIFISYS_PS_TRANSITION=0,1            # Transition occurred from PS0 to PS1