Processing Modes#
The SiWx917 supports different processing modes that affect BLE stack implementation and behavior. Understanding these differences is important for selecting the appropriate mode for your application.
Stack setup and initialization are covered in BLE initialization and configuration.
Mode Overview#
Mode | Description |
|---|---|
Full BLE stack on the Network Processor (NWP); external host over SPI/SDIO/UART through WiSeConnect SDK host library. | |
BLE Controller on the NWP; BLE Host on an external host (for example Linux), HCI between them. | |
Full BLE stack on the NWP; M4 application processor uses WiSeConnect SDK over AHB and shared memory. |
See also: Usage scenarios.
Mode Selection Guidelines#
Choose NCP Mode When:
External host has limited processing capability
Simple integration is preferred
Full BLE stack features needed without host implementation
Host doesn't need BLE stack control
Choose RCP Mode When:
Host has existing BLE host stack implementation
Standard HCI interface preferred
Custom host stack features needed
Host is capable MPU (Linux, etc.)
Choose SoC/ACP Mode When:
Single-chip solution preferred
Low latency requirements
Integrated M4 + NWP solution
Power efficiency is critical
API Compatibility:
NCP and SoC modes: Use WiSeConnect SDK BLE APIs (
rsi_ble_*functions)RCP mode: Uses standard Bluetooth HCI commands (not WiSeConnect SDK APIs)
Implementation details differ but functionality is equivalent
Mode-specific considerations mainly affect integration and API access method
Reference: See the WiSeConnect SDK BLE API Reference for API documentation.