Flash Debugging and Error Handling#
Use this section to troubleshoot flash bring-up and configuration issues on the SiWx917 platform.
Flash initialization, configuration, and command sequencing are controlled exclusively by the Network Wireless Processor (NWP) Bootloader. Developers cannot modify flash settings at runtime. As a result, debugging focuses on verifying the Master Boot Record (MBR), checking device connections, and validating the boot flow using available tools such as Simplicity Studio and Commander.
Because the Bootloader owns all flash operations, there are no APIs for runtime flash reconfiguration, no debug hooks in the NWP flash controller, and no error codes returned during early boot. This makes proper MBR setup critical for system stability.
Common Debugging Tips#
For application-level debugging, see the WiSeConnect Debugging Guide.
Flash debugging focuses on validating the boot path and ensuring that the Bootloader can correctly interpret MBR contents. Typical issues include:
Incorrect flash type or density fields
Incorrect read command or dummy cycle configuration
Incorrect Quad Serial Peripheral Interface (QSPI) mode or frequency selection
Invalid region sizes or address mapping
Corrupted or partially written MBR
Debugging Flash Configuration#
Debugging flash configuration involves validating the MBR, reading back flash contents, and observing boot behavior. Unlike I²C, there is no bus-level waveform debugging available to show command sequencing, because the Bootloader controls all flash accesses internally.
Step 1: Visual Inspection and Connection Checklist#
Before testing MBR or firmware behavior, verify the physical flash interface:
QSPI lines (CLK, CS#, IO0–IO3 or IO0–IO7) are correctly routed to the external flash.
I/O voltage matches the flash device requirements (commonly 1.8 V or 3.3 V).
Power rails are stable during reset and boot.
Timing requirements (power-up delay, reset polarity, tPU) are met.
The correct flash device is populated on the board (density, JEDEC ID, command set).
Issues at this stage often result in a complete boot failure, because the Bootloader cannot perform the initial flash read.
Step 2: Verify the MBR Contents#
The most important step when debugging flash issues is confirming that the MBR is written correctly. The Bootloader:
Reads the MBR immediately after reset
Configures the QSPI controller based solely on its fields
Has no fallback or recovery if the MBR is invalid
To use Silicon Labs Commander to verify the MBR, complete the following steps:
Connect the SiWx917 target device to the host PC.
Open Commander and select the connected device.
Read back the MBR from the device in JSON format.
Verify fields such as:
Flash device type
Density (size)
Read command and dummy cycles
Bus mode (single, dual, quad, or octal)
AES settings (if enabled)
Region definitions and address boundaries
Ensure these values match the flash vendor data sheet and system requirements.
Tip: Always keep a known-good MBR binary in version control. Comparing read-back data against a reference file helps detect corruption quickly.
Step 3 Debug Boot Flow with Simplicity Studio#
Although the Bootloader itself cannot be debugged, you can infer flash configuration failures from system boot behavior:
The device does not reach the application
The device reboots repeatedly
No Universal Asynchronous Receiver/Transmitter (UART) or log output is observed after reset
The device remains in NWP ROM fallback mode, if applicable
Workflow
Connect to Simplicity Studio and select Debug Adapters.
Observe the reset behavior and availability of the device.
If the device cannot load the application image:
Re-read the MBR
Reflash the image
Validate QSPI parameters
Verify flash signal integrity
If ROM logging is enabled, the device console in Simplicity Studio may display Bootloader messages, depending on the device configuration.
Step 4: Using a Logic Analyzer (Optional, Rarely Needed)#
Because flash signals are driven by the Bootloader and not by application firmware, logic analyzer usage is limited. However, captures may help diagnose the following issues:
Incorrect voltage levels
Non-responsive flash device
Misaligned power-up timing
Missing pull-ups on HOLD# or WP# pins
QSPI mode mismatch (for example, the flash expects quad mode but the Bootloader is configured for single mode)
Capture CLK, CS#, and IO0–IO3 lines during early boot to confirm that the Bootloader is issuing valid read commands.
Note: The Bootloader begins issuing flash commands within microseconds of reset. A high-speed logic analyzer with a sample rate of at least 100 MHz is recommended.
Error Code Handling#
Flash operations during boot do not return status codes to the user. If the Bootloader encounters any of the following conditions:
Invalid MBR
Unsupported flash device
Incorrect dummy cycles
Wrong addressing mode
Corrupted configuration fields
The system cannot recover and will fail to boot.
This behavior makes pre-deployment MBR validation essential.
What You Can Do#
Because no runtime error codes are available, use the following strategies to detect and prevent flash issues.
Validate the MBR Before Programming the Device#
Use Commander to compare the written MBR against a known-good binary.
Perform a Flash Sanity Check After Programming#
Read back the first several sectors, including:
The MBR header
The flash configuration block
The application image header
Reinitialize the Flash Image#
If the MBR is corrupted, reprogram it using Commander:
commander flash write mbr.bin --address <MBR_OFFSET>
commander flash write app.bin --address <APP_OFFSET>Check for Layout or Address Overlap#
Incorrect region sizes can cause the Bootloader to load data from the wrong offset.
Check the Flash Vendor Data Sheet#
Mismatches in the following parameters will prevent the Bootloader from reading instructions:
Read opcode
Dummy cycles
Bus width
Quad-enable (QE) bit
Additional Debugging Tips#
Use these practices to improve flash reliability:
Keep the QSPI clock frequency at or below the flash vendor's recommended maximum.
Confirm correct polarity and phase (CPOL and CPHA settings are defined in the MBR).
Avoid partial writes to flash sectors that contain MBR fields.
Ensure flash erase and program operations during manufacturing complete fully; interrupted programming often corrupts the MBR.
Power-cycle the board after flashing the MBR to ensure the Bootloader reloads configuration settings.