Performance Results#
The following table shows the test environment details.
Device | SiWG917 BRD4338A radio board |
Memory Config |
|
AP Used |
|
Environment | RF Shield room |
The following table shows the 11ax throughput results for the above mentioned test environment with SiWG917 in station mode.
S.No | Protocol | Throughput (in Mbps) - Asynchronous |
---|---|---|
1 | UDP Tx | 66 |
2 | UDP Rx | 62 |
3 | TCP Tx | 56 |
4 | TCP Rx | 48 |
5 | TLS Tx | 20 |
6 | TLS Rx | 13 |
The following table shows the throughput results with SiWG917 in access point mode.
S.No | Protocol | Throughput (in Mbps) - Asynchronous |
---|---|---|
1 | UDP Tx | 22.7 |
2 | UDP Rx | 46 |
3 | TCP Tx | 24.7 |
4 | TCP Rx | 20.2 |