Generic SPI#


Introduction#

The Generic SPI Primary (GSPI) is available for MCU HP peripherals and provides an I/O interface for a wide range of SPI-compatible peripheral devices. SPI is a synchronous four-wire interface composed of two data pins (MOSI and MISO), a device select pin (CSN), and a gated clock pin (SCLK). With its two data pins, GSPI supports full-duplex operation with other SPI-compatible devices. GSPI can be utilized in various applications within embedded systems where high-speed, synchronous serial communication is essential. Common use cases include:

  1. Test and Measurement Equipment

  2. Sensor Interfacing

  3. Display Interfaces

  4. Memory Devices

  5. Communication Interfaces

  6. Motor Control

  7. Audio Processing

  8. Wireless Communication

The GSPI controller's internal architecture is depicted in the block diagram below. The following diagram provides a visual representation of the key components and their interactions within the GSPI controller.

GSPI Block DiagramGSPI Block Diagram


Configuration#

Configuring the GSPI in a microcontroller involves several steps, including setting up the peripheral registers, configuring GPIO pins, and selecting the appropriate operating mode and settings. To configure the GSPI operating mode:

The following images illustrate the GSPI bus operations. The first image shows the waveform for a GSPI write operation, detailing how data is transmitted from the primary to the secondary. The second image depicts the waveform for a GSPI read operation, highlighting how data is received from the secondary to the primary.

GSPI bus write operation waveform: This diagram illustrates the sequence of signals during a write operation, including the timing of the clock, data, and chip select signals.

GSPI Write OperationGSPI Write Operation

GSPI bus read operation waveform: This diagram shows the timing and sequence of signals during a read operation, highlighting how data is transferred from the secondary to the primary.

GSPI Read OperationGSPI Read Operation


Usage#

After specifying the GSPI configuration through the sl_gspi_control_config_t structure, you can use the following common GSPI functions to initiate and configure GSPI:

  1. sl_si91x_gspi_init - Initializes the GSPI module.

  2. sl_si91x_gspi_set_configuration - Sets the GSPI configuration.

  3. sl_si91x_gspi_register_event_callback - Registers a callback for GSPI events.

  4. sl_si91x_gspi_send_data - Sends data using the GSPI.

  5. sl_si91x_gspi_receive_data - Receives data using the GSPI.

  6. sl_si91x_gspi_transfer_data - Transfers data using the GSPI.

  7. sl_si91x_gspi_deinit - De-initializes the GSPI module.

Modules#

sl_gspi_control_config_t

sl_gspi_clock_config_t

sl_gspi_version_t

Enumerations#

enum
SL_GSPI_TRANSFER_COMPLETE = ARM_SPI_EVENT_TRANSFER_COMPLETE
SL_GSPI_DATA_LOST = ARM_SPI_EVENT_DATA_LOST
SL_GSPI_MODE_FAULT = ARM_SPI_EVENT_MODE_FAULT
}

Enumeration for different GSPI callback events.

enum
SL_GSPI_POWER_OFF = ARM_POWER_OFF
SL_GSPI_LOW_POWER = ARM_POWER_LOW
SL_GSPI_FULL_POWER = ARM_POWER_FULL
SL_GSPI_POWER_MODE_LAST
}

Enumeration for GSPI power states.

enum
SL_GSPI_MODE_0 = ARM_SPI_CPOL0_CPHA0
SL_GSPI_MODE_3 = ARM_SPI_CPOL1_CPHA1
}

Enumeration for GSPI clock modes.

enum
SL_GSPI_MASTER_INACTIVE = ARM_SPI_MODE_INACTIVE
SL_GSPI_MASTER_ACTIVE = ARM_SPI_MODE_MASTER
SL_GSPI_MASTER_MODE_LAST
}

Enumeration for GSPI primary modes.

enum
SL_GSPI_MASTER_UNUSED = ARM_SPI_SS_MASTER_UNUSED
SL_GSPI_MASTER_SW = ARM_SPI_SS_MASTER_SW
SL_GSPI_MASTER_HW_OUTPUT = ARM_SPI_SS_MASTER_HW_OUTPUT
SL_GSPI_SLAVE_SELECT_MODE_LAST
}

Enumeration for GSPI secondary select modes.

enum
SL_GSPI_MASTER
SL_GSPI_INSTANCE_LAST_ENUM
}

Enumeration for GSPI Primary instance.

enum
GSPI_SLAVE_0
GSPI_SLAVE_1
GSPI_SLAVE_2
GSPI_SLAVE_LAST_ENUM
}

Enumeration for GSPI slave numbers.

Typedefs#

typedef ARM_SPI_SignalEvent_t

Renamed signal event structure.

typedef ARM_SPI_STATUS

Renamed status structure.

typedef ARM_DRIVER_SPI

Renamed GSPI driver structure.

typedef const void *

Created GSPI handle type.

Functions#

sl_status_t
sl_si91x_gspi_configure_clock(sl_gspi_clock_config_t *clock_configuration)

This API is no longer supported due to the restriction on peripheral drivers to configuring clocks.

sl_status_t
sl_si91x_gspi_init(sl_gspi_instance_t instance, sl_gspi_handle_t *gspi_handle)

To initialize the GSPI module.

sl_status_t
sl_si91x_gspi_deinit(sl_gspi_handle_t gspi_handle)

To uninitialize the GSPI module.

sl_status_t
sl_si91x_gspi_set_configuration(sl_gspi_handle_t gspi_handle, sl_gspi_control_config_t *control_configuration)

To configure the GSPI module.

sl_status_t
sl_si91x_gspi_receive_data(sl_gspi_handle_t gspi_handle, void *data, uint32_t data_length)

To receive data from the secondary device.

sl_status_t
sl_si91x_gspi_send_data(sl_gspi_handle_t gspi_handle, const void *data, uint32_t data_length)

To send data to the secondary device.

sl_status_t
sl_si91x_gspi_transfer_data(sl_gspi_handle_t gspi_handle, const void *data_out, void *data_in, uint32_t data_length)

To send and receive data to and from the secondary device simultaneously.

sl_status_t
sl_si91x_gspi_set_master_state(sl_gspi_handle_t gspi_handle, boolean_t value)

To set the primary state as active or inactive.

sl_status_t
sl_si91x_gspi_register_event_callback(sl_gspi_handle_t gspi_handle, sl_gspi_signal_event_t callback_event)

To register the user callback function for GSPI events.

void

To unregister the user callback function for GSPI events.

To fetch the GSPI version.

sl_si91x_gspi_get_status(sl_gspi_handle_t gspi_handle)

To get the transfer status of GSPI.

uint32_t
sl_si91x_gspi_get_rx_data_count(sl_gspi_handle_t gspi_handle)

To fetch the data receive count of the GSPI.

uint32_t

To get the transmit data count of GSPI.

int32_t
sl_si91x_gspi_get_clock_division_factor(sl_gspi_handle_t gspi_handle)

To fetch the clock division factor.

uint32_t

To fetch the frame length, i.e., bit width.

__STATIC_INLINE sl_status_t

To set the secondary number in multi-secondary operation.

Enumeration Documentation#

gspi_event_typedef_t#

gspi_event_typedef_t

Enumeration for different GSPI callback events.

This enumeration defines the possible events that can trigger a GSPI callback. Each event corresponds to a specific condition or state in the GSPI operation.

Enumerator
SL_GSPI_TRANSFER_COMPLETE

Transfer complete event.

SL_GSPI_DATA_LOST

Data lost event.

SL_GSPI_MODE_FAULT

Mode fault event.


sl_gspi_power_state_t#

sl_gspi_power_state_t

Enumeration for GSPI power states.

This enumeration defines the possible power states for the GSPI peripheral. Each state corresponds to a specific power mode that the GSPI can operate in.

Enumeration for GSPI power states.

Enumerator
SL_GSPI_POWER_OFF

Power mode OFF.

SL_GSPI_LOW_POWER

Low power mode.

SL_GSPI_FULL_POWER

Full power mode.

SL_GSPI_POWER_MODE_LAST

Last member of enum for validation.


clock_mode_typedef_t#

clock_mode_typedef_t

Enumeration for GSPI clock modes.

This enumeration defines the possible clock modes for the GSPI peripheral. Each mode corresponds to a specific combination of clock polarity (CPOL) and clock phase (CPHA).

Enumerator
SL_GSPI_MODE_0

Mode 0: CPOL0, CPHA0.

SL_GSPI_MODE_3

Mode 3: CPOL1, CPHA1.


master_mode_typedef_t#

master_mode_typedef_t

Enumeration for GSPI primary modes.

This enumeration defines the possible primary modes for the GSPI peripheral. Each mode indicates whether the GSPI is active or inactive in primary mode.

Enumerator
SL_GSPI_MASTER_INACTIVE

Primary mode inactive.

SL_GSPI_MASTER_ACTIVE

Primary mode active.

SL_GSPI_MASTER_MODE_LAST

Last member of enum for validation.


slave_select_mode_typedef_t#

slave_select_mode_typedef_t

Enumeration for GSPI secondary select modes.

This enumeration defines the possible secondary select modes for the GSPI peripheral. Each mode indicates how the secondary select (SS) signal is managed in primary mode.

Enumerator
SL_GSPI_MASTER_UNUSED

Primary unused mode.

SL_GSPI_MASTER_SW

Primary software mode.

SL_GSPI_MASTER_HW_OUTPUT

Primary hardware output mode.

SL_GSPI_SLAVE_SELECT_MODE_LAST

Last member of enum for validation.


sl_gspi_instance_t#

sl_gspi_instance_t

Enumeration for GSPI Primary instance.

This enumeration defines the GSPI Primary instance. It currently has one member, with a provision for future expansion.

Enumerator
SL_GSPI_MASTER

GSPI Primary instance.

SL_GSPI_INSTANCE_LAST_ENUM

Last member of the enum for validation.


sl_gspi_slave_number_t#

sl_gspi_slave_number_t

Enumeration for GSPI slave numbers.

This enumeration defines the possible slave numbers for the GSPI peripheral. Each value represents a specific slave device connected to the GSPI.

Enumerator
GSPI_SLAVE_0

Secondary No. 0.

GSPI_SLAVE_1

Secondary No. 1.

GSPI_SLAVE_2

Secondary No. 2.

GSPI_SLAVE_LAST_ENUM

Last member of enum for validation.


Typedef Documentation#

sl_gspi_signal_event_t#

typedef ARM_SPI_SignalEvent_t sl_gspi_signal_event_t

Renamed signal event structure.


sl_gspi_status_t#

typedef ARM_SPI_STATUS sl_gspi_status_t

Renamed status structure.


sl_gspi_driver_t#

typedef ARM_DRIVER_SPI sl_gspi_driver_t

Renamed GSPI driver structure.


sl_gspi_handle_t#

typedef const void* sl_gspi_handle_t

Created GSPI handle type.


Function Documentation#

sl_si91x_gspi_configure_clock#

sl_status_t sl_si91x_gspi_configure_clock (sl_gspi_clock_config_t * clock_configuration)

This API is no longer supported due to the restriction on peripheral drivers to configuring clocks.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_clock_config_t *[in]clock_configuration

Pointer to the clock configuration structure sl_gspi_clock_config_t.

To configure the clock for the GSPI module.

This API sets the clock for the GSPI peripheral. It configures the PLL clock and SOC clock according to the values set by the user in the clock configuration structure.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_init#

sl_status_t sl_si91x_gspi_init (sl_gspi_instance_t instance, sl_gspi_handle_t * gspi_handle)

To initialize the GSPI module.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_instance_t[in]instance

GSPI instance sl_gspi_instance_t.

sl_gspi_handle_t *[in]gspi_handle

Double pointer to the GSPI driver handle sl_gspi_handle_t.

This API initializes the GSPI module. If DMA is enabled, it also initializes the DMA module. The API takes the address of a pointer to store the GSPI primary handle, which can be used for subsequent function calls.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_deinit#

sl_status_t sl_si91x_gspi_deinit (sl_gspi_handle_t gspi_handle)

To uninitialize the GSPI module.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle sl_gspi_handle_t.

This API uninitializes the GSPI module. If DMA is enabled, it also uninitializes the DMA module.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

For more information on status codes, see SL STATUS DOCUMENTATION.

Note

  • When the GSPI module is used in combination with other peripherals, see the notes below while deinitializing in the application:

    1. Whenever sl_si91x_gspi_deinit() is called, it will disable the clock for the peripheral. To power off the peripheral, you must power down the power domain (PERI_EFUSE), which contains different peripherals mentioned below: USART, UART, I2C, SSI Primary, SSI Secondary, Generic-SPI Primary, I2S Primary, I2S Secondary, Micro-DMA Controller, Config Timer, Random-Number Generator, CRC Accelerator, SIO, QEI, MCPWM, and EFUSE. Use the following API to power down the particular power domain if other peripherals are not being used: sl_si91x_peri_efuse_power_down(power_down);

    2. A few peripherals (ULP Peripherals, UULP Peripherals, GPDMA, and SDIO-SPI) have separate domains; those can be powered down independently. For additional details, see the Power architecture section in the Hardware Reference Manual. For example, ULP_UART has a separate power domain ULPSS_PWRGATE_ULP_UART, which can be powered down independently. Refer to the rsi_power_save.h file for all power gate definitions.


sl_si91x_gspi_set_configuration#

sl_status_t sl_si91x_gspi_set_configuration (sl_gspi_handle_t gspi_handle, sl_gspi_control_config_t * control_configuration)

To configure the GSPI module.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle sl_gspi_handle_t.

sl_gspi_control_config_t *[in]control_configuration

Pointer to the configuration structure sl_gspi_control_config_t.

The GSPI control and configuration options are listed below:

  • swap_read (enable/disable)

  • swap_write (enable/disable)

  • bit_width (1-16 bits)

  • clock_mode (mode0/mode3)

  • slave_select_mode (hw_output/sw)

  • bitrate

Note

  • Swap Read and Swap Write can be used only if the bit_width is configured as 16.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_FAIL - Function failed.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_NOT_SUPPORTED - Parameter is not supported.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

    • SL_STATUS_INVALID_MODE - Secondary select mode is invalid.

    • SL_STATUS_INVALID_TYPE - SPI frame format is not valid.

    • SL_STATUS_INVALID_RANGE - Data bits (frame length) are not in range.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_receive_data#

sl_status_t sl_si91x_gspi_receive_data (sl_gspi_handle_t gspi_handle, void * data, uint32_t data_length)

To receive data from the secondary device.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle sl_gspi_handle_t.

void *[in]data

Pointer to the variable that will store the received data.

uint32_t[in]data_length

(uint32_t) Number of data items to receive.

If DMA is enabled, it configures the DMA channel and required parameters. When the received data is equal to the data_length passed in this function, a callback event is generated which can be registered using sl_si91x_gspi_register_event_callback.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_FAIL - Function failed.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_send_data#

sl_status_t sl_si91x_gspi_send_data (sl_gspi_handle_t gspi_handle, const void * data, uint32_t data_length)

To send data to the secondary device.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle sl_gspi_handle_t.

const void *[in]data

Const pointer to the variable that contains the data to be sent.

uint32_t[in]data_length

(uint32_t) Number of data items to send.

If DMA is enabled, it configures the DMA channel and required parameters. When the sent data is equal to the data_length passed in this function, a callback event is generated which can be registered using sl_si91x_gspi_register_event_callback.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_FAIL - Function failed.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_transfer_data#

sl_status_t sl_si91x_gspi_transfer_data (sl_gspi_handle_t gspi_handle, const void * data_out, void * data_in, uint32_t data_length)

To send and receive data to and from the secondary device simultaneously.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle sl_gspi_handle_t.

const void *[in]data_out

Const pointer to the variable that has data which needs to be sent.

void *[in]data_in

Pointer to the variable that will store the received data.

uint32_t[in]data_length

(uint32_t) Number of data items to receive.

If DMA is enabled, it configures the DMA channel and required parameters. When the received data and sent data are equal to the data_length passed in this function, a callback event is generated which can be registered using sl_si91x_gspi_register_event_callback.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_FAIL - Function failed.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_set_master_state#

sl_status_t sl_si91x_gspi_set_master_state (sl_gspi_handle_t gspi_handle, boolean_t value)

To set the primary state as active or inactive.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle sl_gspi_handle_t.

boolean_t[in]value

(boolean_t) Enable or Disable.

Sets the primary state (i.e., activate/deactivate). If the primary is not required in the application for a specific time, it can be turned on/off at runtime by using this API.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

    • SL_STATUS_INVALID_MODE - Mode is invalid (fails to activate primary).

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_register_event_callback#

sl_status_t sl_si91x_gspi_register_event_callback (sl_gspi_handle_t gspi_handle, sl_gspi_signal_event_t callback_event)

To register the user callback function for GSPI events.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle ( sl_gspi_handle_t).

sl_gspi_signal_event_t[in]callback_event

Pointer to the function that needs to be called at the time of interrupt ( sl_gspi_signal_event_t).

At the time of the event, the function passed in the parameter is called with the respective event as the parameter. Before calling this function again, it is mandatory to call the sl_si91x_gspi_unregister_event_callback function to unregister the callback; otherwise, it returns SL_STATUS_BUSY error code.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success.

    • SL_STATUS_BUSY - Driver is busy.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gspi_unregister_event_callback#

void sl_si91x_gspi_unregister_event_callback (void )

To unregister the user callback function for GSPI events.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API unregisters the user callback function that was previously registered using sl_si91x_gspi_register_event_callback. It is mandatory to call this function before registering the callback again to avoid conflicts.


sl_si91x_gspi_get_version#

sl_gspi_version_t sl_si91x_gspi_get_version (void )

To fetch the GSPI version.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API reads and returns the current API version of GSPI.

Returns


sl_si91x_gspi_get_status#

sl_gspi_status_t sl_si91x_gspi_get_status (sl_gspi_handle_t gspi_handle)

To get the transfer status of GSPI.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle ( sl_gspi_handle_t).

This API returns the sl_gspi_status_t type structure. The members are:

  • Busy

  • Data Lost

  • Mode Fault It is used to poll the busy status of the GSPI Primary.

Returns


sl_si91x_gspi_get_rx_data_count#

uint32_t sl_si91x_gspi_get_rx_data_count (sl_gspi_handle_t gspi_handle)

To fetch the data receive count of the GSPI.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle ( sl_gspi_handle_t).

If a receive operation is started, this function can be used to get the number of data bytes received.

Returns

  • uint32_t value of the RX data count.


sl_si91x_gspi_get_tx_data_count#

uint32_t sl_si91x_gspi_get_tx_data_count (void )

To get the transmit data count of GSPI.

Parameters
TypeDirectionArgument NameDescription
voidN/A

If a send operation is started, this function can be used to get the number of data bytes sent.

Returns

  • uint32_t Value of the TX data count.


sl_si91x_gspi_get_clock_division_factor#

int32_t sl_si91x_gspi_get_clock_division_factor (sl_gspi_handle_t gspi_handle)

To fetch the clock division factor.

Parameters
TypeDirectionArgument NameDescription
sl_gspi_handle_t[in]gspi_handle

Pointer to the GSPI driver handle ( sl_gspi_handle_t).

The clock division factor is calculated based on the configured peripheral clock. It determines the baud rate of GSPI.

Returns

  • factor (int32_t) The value of the clock division factor.


sl_si91x_gspi_get_frame_length#

uint32_t sl_si91x_gspi_get_frame_length (void )

To fetch the frame length, i.e., bit width.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API fetches the frame length. The frame length ranges between 1 and 15.

Returns

  • frame_length (uint32_t) The value of the frame length.


sl_si91x_gspi_set_slave_number#

__STATIC_INLINE sl_status_t sl_si91x_gspi_set_slave_number (uint8_t number)

To set the secondary number in multi-secondary operation.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]number

Secondary number ( sl_gspi_slave_number_t).

For a single secondary, this API needs to be called before transferring the data.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success

    • SL_STATUS_INVALID_PARAMETER - Invalid parameter

For more information on status codes, see SL STATUS DOCUMENTATION.