Structure to hold the clock configuration members for the GSPI peripheral.
This structure contains the clock configuration members for the GSPI peripheral, including SoC PLL count value, interface PLL control value, clock frequencies, and division factor.
Public Attributes#
uint8_t
SoC PLL count value.
uint16_t
Interface PLL control value.
uint32_t
Interface PLL clock frequency.
uint32_t
Interface PLL reference clock frequency.
uint32_t
SoC PLL clock frequency.
uint32_t
SoC PLL reference clock frequency.
uint16_t
Clock division factor.
Public Attribute Documentation#
intf_pll_500_control_value#
uint16_t sl_gspi_clock_config_t::intf_pll_500_control_value
Interface PLL control value.
intf_pll_reference_clock#
uint32_t sl_gspi_clock_config_t::intf_pll_reference_clock
Interface PLL reference clock frequency.
soc_pll_reference_clock#
uint32_t sl_gspi_clock_config_t::soc_pll_reference_clock
SoC PLL reference clock frequency.