You are viewing documentation for version:
PDFStructure to hold the parameters for the configuration of the SSI peripheral.
Public Attributes#
uint32_t
Mode such as Master or Slave mode.
uint32_t
Clock mode such as CPOL0 CPHA1.
uint32_t
Delay for the receive input signal.
uint32_t
Transfer mode: single, dual, or quad line.
Public Attribute Documentation#
bit_width#
uint8_t sl_ssi_control_config_t::bit_width
Bit width, 4 - 16 bits.
device_mode#
uint32_t sl_ssi_control_config_t::device_mode
Mode such as Master or Slave mode.
clock_mode#
uint32_t sl_ssi_control_config_t::clock_mode
Clock mode such as CPOL0 CPHA1.
baud_rate#
uint32_t sl_ssi_control_config_t::baud_rate
Baud rate for SSI.
receive_sample_delay#
uint32_t sl_ssi_control_config_t::receive_sample_delay
Delay for the receive input signal.
transfer_mode#
uint32_t sl_ssi_control_config_t::transfer_mode
Transfer mode: single, dual, or quad line.