Structure to hold the parameters for Watchdog Timer clock source configurations.
This structure contains the configuration parameters for the Watchdog Timer's clock sources, including low frequency FSM clock source, high frequency FSM clock source, and BG-PMU clock source.
Public Attributes#
uint8_t
Low frequency FSM clock source, see low_freq_fsm_clock_t.
uint8_t
High frequency FSM clock source, see high_freq_fsm_clock_t.
uint8_t
BG-PMU clock source.
Public Attribute Documentation#
low_freq_fsm_clock_src#
uint8_t watchdog_timer_clock_config_t::low_freq_fsm_clock_src
Low frequency FSM clock source, see low_freq_fsm_clock_t.
Definition at line
118
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h
high_freq_fsm_clock_src#
uint8_t watchdog_timer_clock_config_t::high_freq_fsm_clock_src
High frequency FSM clock source, see high_freq_fsm_clock_t.
Definition at line
119
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h
bg_pmu_clock_source#
uint8_t watchdog_timer_clock_config_t::bg_pmu_clock_source
BG-PMU clock source.
Definition at line
120
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h