TWT (Target Wake Time) reschedule configuration structure.
Public Attributes#
uint8_t
TWT session flow ID.
Specifies the action need to be taken for rescheduling the TWT session. This determines how and when the TWT session would be suspended or adjusted. See sl_wifi_reschedule_twt_action_t for the possible actions.
uint16_t
Reserved.
uint8_t
Reserved.
uint64_t
Duration to suspend the respective TWT session, in microseconds.
Public Attribute Documentation#
flow_id#
uint8_t sl_wifi_reschedule_twt_config_t::flow_id
TWT session flow ID.
Definition at line
523
of file components/protocol/wifi/inc/sl_wifi_types.h
twt_action#
sl_wifi_reschedule_twt_action_t sl_wifi_reschedule_twt_config_t::twt_action
Specifies the action need to be taken for rescheduling the TWT session. This determines how and when the TWT session would be suspended or adjusted. See sl_wifi_reschedule_twt_action_t for the possible actions.
Definition at line
525
of file components/protocol/wifi/inc/sl_wifi_types.h
reserved1#
uint16_t sl_wifi_reschedule_twt_config_t::reserved1
Reserved.
Definition at line
526
of file components/protocol/wifi/inc/sl_wifi_types.h
reserved2#
uint8_t sl_wifi_reschedule_twt_config_t::reserved2
Reserved.
Definition at line
527
of file components/protocol/wifi/inc/sl_wifi_types.h
suspend_duration#
uint64_t sl_wifi_reschedule_twt_config_t::suspend_duration
Duration to suspend the respective TWT session, in microseconds.
Definition at line
528
of file components/protocol/wifi/inc/sl_wifi_types.h