Wi-Fi scan configuration structure.
Indicates the configuration parameters for a Wi-Fi scan operation.
Note
The Quick Scan feature is enabled when a specific channel and SSID are given for scanning. SiWx91x scans for the AP given in the scan API and posts the scan results immediately after finding the access point.
The
channel_bitmap_2g4
uses the lower 14 bits to represent channels from 1 to 14, where channel 1 = (1 << 0), channel 2 = (1 << 1), and so on.5GHz is not supported.
Channel Number 2.4 GHz | channel_bitmap_2g4 |
---|---|
1 | (1 << 0) |
2 | (1 << 1) |
3 | (1 << 2) |
4 | (1 << 3) |
5 | (1 << 4) |
6 | (1 << 5) |
7 | (1 << 6) |
8 | (1 << 7) |
9 | (1 << 8) |
10 | (1 << 9) |
11 | (1 << 10) |
12 | (1 << 11) |
13 | (1 << 12) |
14 | (1 << 13) |
Public Attributes#
Scan type to be configured of type sl_wifi_scan_type_t.
Reserved.
Duration in milliseconds between periodic scans.
Bitmap of selected 2.4 GHz channels.
Bitmap of selected 5 GHz channels (currently not supported)
Enable LP mode, 1 - Enable LP mode, 0 - Disable LP mode.
Public Attribute Documentation#
type#
sl_wifi_scan_type_t sl_wifi_scan_configuration_t::type
Scan type to be configured of type sl_wifi_scan_type_t.
250
of file components/protocol/wifi/inc/sl_wifi_types.h
flags#
uint32_t sl_wifi_scan_configuration_t::flags
Reserved.
251
of file components/protocol/wifi/inc/sl_wifi_types.h
periodic_scan_interval#
uint32_t sl_wifi_scan_configuration_t::periodic_scan_interval
Duration in milliseconds between periodic scans.
252
of file components/protocol/wifi/inc/sl_wifi_types.h
channel_bitmap_2g4#
uint16_t sl_wifi_scan_configuration_t::channel_bitmap_2g4
Bitmap of selected 2.4 GHz channels.
253
of file components/protocol/wifi/inc/sl_wifi_types.h
channel_bitmap_5g#
uint32_t sl_wifi_scan_configuration_t::channel_bitmap_5g[8]
Bitmap of selected 5 GHz channels (currently not supported)
254
of file components/protocol/wifi/inc/sl_wifi_types.h
lp_mode#
uint8_t sl_wifi_scan_configuration_t::lp_mode
Enable LP mode, 1 - Enable LP mode, 0 - Disable LP mode.
255
of file components/protocol/wifi/inc/sl_wifi_types.h