Troubleshoot#

  • Facing peripheral functionality issues after migration

    • Cross-check the pin mapping in the respective peripheral component configurations, or the <project_name>/config files.

  • Both old and new SDK contents are visible after importing the project. Followed by build error stating Make File Not Found

    • Make sure the imported project name is same as the previous project.

  • Build errors because of missing files, such as Target Not Found

    • Open <project_name>.slcp and perform force generation as shown in the following image. This step regenerates the project with the SDK files.

    Note:#

    Cross-check the /autogen and /config folder contents after Force Generation, as they might be replaced with the default SDK files.

    Force GenerationForce Generation