Modules#
CoAP#
The Wi-SUN CoAP component provides an application layer implementation on top of the Wi-SUN stack and its socket API. The CoAP protocol is designed as a specialized Internet Application Protocol for constrained devices in lossy networks (refer to RFC 7252 for additional information). The Wi-SUN FAN networks fit exactly this definition. The CoAP implementation relies on the UDP transport layer to send and receive packets.
A number of helper functions are part of the component to assist with building CoAP payloads, parsing CoAP packets, comparing URI (Uniform Resource Identifier) paths, freeing CoAP packets, and more. The CoAP component can rely on either a static or dynamic memory pool to store CoAP packets. The dynamic implementation uses OS-dependent memory allocation and memory release APIs. The static implementation is only available when using FreeRTOS.
To use the CoAP component in your application, add it to your project and initialize it with sl_wisun_coap_init().
Functions#
Wi-SUN CoAP init.
Wi-SUN CoAP default init.
Wi-SUN CoAP get lib state.
Wi-SUN CoAP malloc implementation.
Wi-SUN CoAP free.
CoAP parser wrapper function.
CoAP packet calc size wrapper.
CoAP message builder Wi-SUN.
Build generic response for request wrapper function.
Print CoAP packets and all of attached buffer, payload, token, uri_path.
Get last parsed URI path.
Get payload.
Set payload.
Get token.
Set token.
Get options list.
Set options list.
Get library handler pointer from internal handler structure.
Destroy packet.
Compare URI path with the stored from previous parsed packet.
Function Documentation#
sl_wisun_coap_init#
bool sl_wisun_coap_init (const sl_wisun_coap_tx_callback tx_callback, const sl_wisun_coap_rx_callback rx_callback, const sl_wisun_coap_version_t version)
Wi-SUN CoAP init.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_tx_callback | [in] | tx_callback | TX callback, if it's NULL, the default callback is applied |
| const sl_wisun_coap_rx_callback | [in] | rx_callback | RX callback, if it's NULL, the default callback is applied |
| const sl_wisun_coap_version_t | [in] | version | CoAP version |
Set the Wi-SUN CoAP internal descriptor Returns
true Proper initialization
false Error
sl_wisun_coap_init_default#
static bool sl_wisun_coap_init_default (void )
Wi-SUN CoAP default init.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
initialize the internal descriptor with default values Returns
true Proper initialization
false Error
sl_wisun_coap_is_initialized#
bool sl_wisun_coap_is_initialized (void )
Wi-SUN CoAP get lib state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Get initialized state of the CoAP library to decide init is need or not Returns
true Initialized
false Not initialized
sl_wisun_coap_malloc#
void* sl_wisun_coap_malloc (uint16_t size)
Wi-SUN CoAP malloc implementation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | size | size for malloc |
OS dependent thread-safe implementation Returns
void* the memory pointer
sl_wisun_coap_free#
void sl_wisun_coap_free (void * addr)
Wi-SUN CoAP free.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | N/A | addr | address ptr |
OS dependent thread-safe implementation
sl_wisun_coap_parser#
sl_wisun_coap_packet_t* sl_wisun_coap_parser (uint16_t packet_data_len, uint8_t * packet_data)
CoAP parser wrapper function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | packet_data_len | packet data size |
| uint8_t * | [in] | packet_data | packet data ptr |
Used sn_coap_parser
sl_wisun_coap_builder_calc_size#
uint16_t sl_wisun_coap_builder_calc_size (const sl_wisun_coap_packet_t * message)
CoAP packet calc size wrapper.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_packet_t * | [in] | message | message ptr |
Used sn_coap_builder_calc_needed_packet_data_size Returns
uint16_t size
sl_wisun_coap_builder#
int16_t sl_wisun_coap_builder (uint8_t * dest_buff, const sl_wisun_coap_packet_t * message)
CoAP message builder Wi-SUN.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | dest_buff | destination buffer for raw message |
| const sl_wisun_coap_packet_t * | [in] | message | message structure |
Used sl_wisun_coap_builder Returns
int16_t On success bytes of built message, on failure -1 if coap header structure is wrong -2 if NULL ptr set as argument
sl_wisun_coap_build_response#
sl_wisun_coap_packet_t* sl_wisun_coap_build_response (const sl_wisun_coap_packet_t * req, sl_wisun_coap_message_code_t msg_code)
Build generic response for request wrapper function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_packet_t * | [in] | req | request |
| sl_wisun_coap_message_code_t | [in] | msg_code | message code to build |
Used sn_coap_build_response Returns
sl_wisun_coap_header_t* built packet ptr on the heap
sl_wisun_coap_print_packet#
void sl_wisun_coap_print_packet (const sl_wisun_coap_packet_t * packet, const bool hex_format)
Print CoAP packets and all of attached buffer, payload, token, uri_path.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_packet_t * | [in] | packet | packet to print |
| const bool | [in] | hex_format | hex format bool to decide buffer print format |
Pretty printer function, with hex format option for buffers
sl_wisun_coap_get_parsed_uri_path#
const char* sl_wisun_coap_get_parsed_uri_path (char * dest_buff, const uint16_t buff_length)
Get last parsed URI path.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| char * | N/A | dest_buff | destination buff |
| const uint16_t | N/A | buff_length | destination buffer size |
Thread safe way to get the URI path from last parsed packet Returns
const char* On success, pointer to the destination buffer, NULL on failure
sl_wisun_coap_get_payload#
bool sl_wisun_coap_get_payload (const sl_wisun_coap_packet_t * source_packet, uint8_t * dest_buff, const uint16_t buff_length)
Get payload.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_packet_t * | [in] | source_packet | source packet |
| uint8_t * | [out] | dest_buff | destination buffer |
| const uint16_t | [in] | buff_length | length of destination buffer |
Thread safe deep copy Returns
true Success
false Failure
sl_wisun_coap_set_payload#
void sl_wisun_coap_set_payload (sl_wisun_coap_packet_t * dest_packet, uint8_t * source_buff, const uint16_t buff_length)
Set payload.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_coap_packet_t * | [out] | dest_packet | destination packet |
| uint8_t * | [in] | source_buff | source buffer |
| const uint16_t | [in] | buff_length | source buffer length |
Set the corresponding packet member ptr and length
sl_wisun_coap_get_token#
bool sl_wisun_coap_get_token (const sl_wisun_coap_packet_t * source_packet, uint8_t * dest_buff, const uint16_t buff_length)
Get token.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_packet_t * | [in] | source_packet | source packet |
| uint8_t * | [out] | dest_buff | destination buffer |
| const uint16_t | [in] | buff_length | length of destination buffer |
Thread safe deep copy Returns
true Success
false Failure
sl_wisun_coap_set_token#
void sl_wisun_coap_set_token (sl_wisun_coap_packet_t * dest_packet, uint8_t * source_buff, const uint8_t buff_length)
Set token.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_coap_packet_t * | N/A | dest_packet | destination packet |
| uint8_t * | N/A | source_buff | source buffer |
| const uint8_t | N/A | buff_length | source buffer length |
Set the corresponding packet member ptr and length
sl_wisun_coap_get_options_list#
bool sl_wisun_coap_get_options_list (const sl_wisun_coap_packet_t * source_packet, sl_wisun_coap_option_list_t * dest)
Get options list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_coap_packet_t * | N/A | source_packet | source packet |
| sl_wisun_coap_option_list_t * | N/A | dest | destination option list structure |
Thread safe deep copy Returns
true Success
false Failure
sl_wisun_coap_set_options_list#
void sl_wisun_coap_set_options_list (sl_wisun_coap_packet_t * dest_packet, sl_wisun_coap_option_list_t * source)
Set options list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_coap_packet_t * | [out] | dest_packet | destination packet ptr |
| sl_wisun_coap_option_list_t * | [in] | source | source option list |
Set the option list pointer.
sl_wisun_coap_get_lib_handler#
const sl_wisun_coap_handle_t* sl_wisun_coap_get_lib_handler (void )
Get library handler pointer from internal handler structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Not thread safe! It is needed only to use Pelion mbed-coap library functions Returns
const sl_wisun_coap_handle_t* pointer to the lib handler
sl_wisun_coap_destroy_packet#
void sl_wisun_coap_destroy_packet (sl_wisun_coap_packet_t * packet)
Destroy packet.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_coap_packet_t * | N/A | packet | packet |
It must be used to avoid memory leaks! Free the all of allocated buffer for packet
sl_wisun_coap_compare_uri_path#
bool sl_wisun_coap_compare_uri_path (const char * uri_path, const uint16_t buff_max_len)
Compare URI path with the stored from previous parsed packet.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | N/A | uri_path | URI path |
| const uint16_t | N/A | buff_max_len | buffer size of the URI path |
Thread safe way to compare URI pathes. The buffer length must be set, eg strlen(uri_path) + 1 Returns
true Matched
false Not matched