Modules#
Application Core type definitions
Application Core#
The Application Core component aims at providing utilities common to most Wi-SUN applications. Following this objective, the component offers the following features:
A Wi-SUN connection helper function app_wisun_network_connect(). This function configures the network size setting, the TX output power, the certificates, and keys. The last function action is to start the catual Wi-SUN connection process.
An event handler and callback mechanisms. It provides a thread-safe abstraction layer on the Wi-SUN stack events reported in sl_wisun_on_event(). Two APIs (app_wisun_register_custom_callback() and app_wisun_remove_custom_callback()) are exposed to the application to add or remove custom callbacks associated with stack events.
A ping capability through the app_wisun_ping() function. It can be used to test communications and latencies in a Wi-SUN network.
A Socket FIFO overflow handler. The application can redefine the weakly implemented app_wisun_socket_fifo_overflow_handler() function to handle the socket FIFO overflow events.
A graphical interface in Simplicity Studio to configure the network name, TX power, and network size to be used during the connection process.
To use the component in your application, add it to your project and initialize it with app_wisun_core_init().
Functions#
Initialize Wi-SUN application core.
Connect to the Wi-SUN network.
Disconnect from the Wi-SUN network.
Register custom callback.
Remove custom callback.
Get the connection state.
Ping remote address.
Wi-SUN socket FiFO overflow handler.
Get the IP address.
Function Documentation#
app_wisun_core_init#
void app_wisun_core_init (void )
Initialize Wi-SUN application core.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Init mutex, init socket handler and set Wi-SUN setting
app_wisun_network_connect#
void app_wisun_network_connect (void )
Connect to the Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Network init and connecting.
app_wisun_network_disconnect#
void app_wisun_network_disconnect (void )
Disconnect from the Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Call Wi-SUN disconnect API.
app_wisun_register_custom_callback#
void app_wisun_register_custom_callback (const sl_wisun_msg_ind_id_t id, custom_wisun_event_callback_t custom_callback)
Register custom callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_msg_ind_id_t | [in] | id | sl_wisun_msg_ind_id_t message ID from the stack |
| custom_wisun_event_callback_t | [in] | custom_callback | callback to regist |
Set the custom callback ptr.
app_wisun_remove_custom_callback#
void app_wisun_remove_custom_callback (const sl_wisun_msg_ind_id_t id)
Remove custom callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_msg_ind_id_t | [in] | id | sl_wisun_msg_ind_id_t message id from stack |
set the custom callback ptr
app_wisun_get_connection_state#
wisun_network_connection_state_t app_wisun_get_connection_state (void )
Get the connection state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
set the custom callback ptr to NULL Returns
wisun_network_connection_state_t Connection state
app_wisun_ping#
bool app_wisun_ping (wisun_addr_t *const remote_addr)
Ping remote address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| wisun_addr_t *const | [in] | remote_addr | Remote byte address |
Send ICMP packets to the remote and receive the response. Returns
true if ping was successful
false error
app_wisun_socket_fifo_overflow_handler#
void app_wisun_socket_fifo_overflow_handler (const int32_t socketid, const uint8_t * remaining_buffer, const uint32_t remaining_size)
Wi-SUN socket FiFO overflow handler.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const int32_t | [in] | socketid | socket ID |
| const uint8_t * | [in] | remaining_buffer | remaining buffer ptr |
| const uint32_t | [in] | remaining_size | remeaing size of buffer |
Weak implementation, which can be overridden. Users can create custom backup process to store remaining data.
app_wisun_get_ip_address_str#
const char* app_wisun_get_ip_address_str (const void *const value)
Get the IP address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const void *const | [in] | value | IP address raw byte values. |
Uses the internal circular buffer. Returns
const char* converted string ptr