Connection parameter set.
Public Attributes#
uint16_t
Version of this API.
PAN discovery parameter set.
PAN configuration parameter set.
Authentication parameter set.
RPL parameters set.
MPL parameter set.
Misc parameter set.
Public Attribute Documentation#
version#
uint16_t sl_wisun_connection_params_t::version
Version of this API.
This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.
Definition at line
183
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
discovery#
sl_wisun_params_discovery sl_wisun_connection_params_t::discovery
PAN discovery parameter set.
Definition at line
185
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
configuration#
sl_wisun_params_configuration sl_wisun_connection_params_t::configuration
PAN configuration parameter set.
Definition at line
187
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
eapol#
sl_wisun_params_eapol sl_wisun_connection_params_t::eapol
Authentication parameter set.
Definition at line
189
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
rpl#
sl_wisun_params_rpl sl_wisun_connection_params_t::rpl
RPL parameters set.
Definition at line
191
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
mpl#
sl_wisun_params_mpl sl_wisun_connection_params_t::mpl
MPL parameter set.
Definition at line
193
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
misc#
sl_wisun_params_misc sl_wisun_connection_params_t::misc
Misc parameter set.
Definition at line
195
of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h