Trickle parameters set.

Public Attributes#

uint16_t

Minimum interval size (seconds)

uint16_t

Maximum interval size (seconds)

uint8_t

Redundancy constant (0 for infinity)

Public Attribute Documentation#

imin_s#

uint16_t sl_wisun_trickle_params_t::imin_s

Minimum interval size (seconds)


Definition at line 61 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

imax_s#

uint16_t sl_wisun_trickle_params_t::imax_s

Maximum interval size (seconds)


Definition at line 63 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

k#

uint8_t sl_wisun_trickle_params_t::k

Redundancy constant (0 for infinity)


Definition at line 65 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h