MAC statistics.

Public Attributes#

uint16_t

Current number of frames in the MAC transmission queue.

uint16_t

Highest number of frames in the MAC transmission queue.

uint32_t

Number of successfully received MAC frames.

uint32_t

Number of transmitted MAC frames.

uint32_t

Number of successfully received broadcast MAC frames.

uint32_t

Number of transmitted broadcast MAC frames.

uint32_t

Number of successfully received MAC frames discarded during processing.

uint32_t

Amount of transmitted MAC data in bytes. FCS is not included.

uint32_t

Amount of successfully received MAC data in bytes. FCS is not included.

uint32_t

Number of failed MAC transmissions.

uint32_t

Number of retried MAC transmissions.

uint32_t

Number of MAC CCA attempts.

uint32_t

Number of failed MAC transmissions due to CCA.

uint32_t

Number of successfully received MAC frames using mode_switch.

uint32_t

Number of transmitted MAC frames using mode switch.

uint32_t

Number of failed reception using mode switch (no data after PHR or MDR Command).

uint32_t

Number of failed MAC frames transmission using mode switch.

Public Attribute Documentation#

tx_queue_size#

uint16_t sl_wisun_statistics_mac_t::tx_queue_size

Current number of frames in the MAC transmission queue.


Definition at line 341 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

tx_queue_peak#

uint16_t sl_wisun_statistics_mac_t::tx_queue_peak

Highest number of frames in the MAC transmission queue.


Definition at line 343 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

rx_count#

uint32_t sl_wisun_statistics_mac_t::rx_count

Number of successfully received MAC frames.


Definition at line 345 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

tx_count#

uint32_t sl_wisun_statistics_mac_t::tx_count

Number of transmitted MAC frames.


Definition at line 347 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

bc_rx_count#

uint32_t sl_wisun_statistics_mac_t::bc_rx_count

Number of successfully received broadcast MAC frames.


Definition at line 349 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

bc_tx_count#

uint32_t sl_wisun_statistics_mac_t::bc_tx_count

Number of transmitted broadcast MAC frames.


Definition at line 351 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

rx_drop_count#

uint32_t sl_wisun_statistics_mac_t::rx_drop_count

Number of successfully received MAC frames discarded during processing.


Definition at line 353 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

tx_bytes#

uint32_t sl_wisun_statistics_mac_t::tx_bytes

Amount of transmitted MAC data in bytes. FCS is not included.


Definition at line 355 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

rx_bytes#

uint32_t sl_wisun_statistics_mac_t::rx_bytes

Amount of successfully received MAC data in bytes. FCS is not included.


Definition at line 357 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

tx_failed_count#

uint32_t sl_wisun_statistics_mac_t::tx_failed_count

Number of failed MAC transmissions.


Definition at line 359 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

retry_count#

uint32_t sl_wisun_statistics_mac_t::retry_count

Number of retried MAC transmissions.


Definition at line 361 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

cca_attempts_count#

uint32_t sl_wisun_statistics_mac_t::cca_attempts_count

Number of MAC CCA attempts.


Definition at line 363 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

failed_cca_count#

uint32_t sl_wisun_statistics_mac_t::failed_cca_count

Number of failed MAC transmissions due to CCA.


Definition at line 365 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

rx_ms_count#

uint32_t sl_wisun_statistics_mac_t::rx_ms_count

Number of successfully received MAC frames using mode_switch.


Definition at line 367 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

tx_ms_count#

uint32_t sl_wisun_statistics_mac_t::tx_ms_count

Number of transmitted MAC frames using mode switch.


Definition at line 369 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

rx_ms_failed_count#

uint32_t sl_wisun_statistics_mac_t::rx_ms_failed_count

Number of failed reception using mode switch (no data after PHR or MDR Command).


Definition at line 371 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

tx_ms_failed_count#

uint32_t sl_wisun_statistics_mac_t::tx_ms_failed_count

Number of failed MAC frames transmission using mode switch.


Definition at line 373 of file /mnt/raid/workspaces/ws.0wy4DfJrj/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h