Over-The-Air Device Firmware Upgrade (Alpha)#

Wi-SUN Over-The-Air Device Firmware Upgrade (OTA DFU) service is implemented for updating Wi-SUN device's firmware. The component uses the Gecko Bootloader API to perform firmware write, verify, and set to bootload operations.

A Trivial File Transfer Protocol (TFTP) client provides downloader solution to obtain a new Gecko Bootloader File (GBL) file from remote host Over-The-Air, using the Wi-SUN network. The connection to the TFTP remote host can be configured in component configuration file. The entire firmware upgrade session can be managed over CoAP. The service includes notification and status request capabilities.

The Wi-SUN Over-The-Air Device Firmware Upgrade (OTA DFU) service is implemented to facilitate the updating of Wi-SUN device firmware. This component requires the Gecko Bootloader API to execute firmware writing, verification, and boot-load operations.

To obtain a new Gecko Bootloader File (GBL) file from a remote host Over-The-Air, a Trivial File Transfer Protocol (TFTP) client is employed, leveraging the Wi-SUN network. The entire firmware upgrade session is manageable over CoAP, with the service offering remote host connection settings, firmware file selection, notification and status request capabilities. Configuration of the connection to the TFTP remote host can be accomplished even within the component configuration file. To utilize this component, a bootloader must be flashed onto the device. The component relies on functions that reside within the bootloader. To choose the appropriate bootloader, consider factors such as flash location (internal or external) and size. If necessary, apply compression.

Modules#

Type definitions

Functions#

void
sl_wisun_ota_dfu_error_hnd(const sl_wisun_ota_dfu_error_code_t error_code, sl_wisun_ota_dfu_error_ctx_t *const ctx)

OTA DFU error handler (weak implementation)

void

Free the status string buffer.

uint32_t

Get the status value.

bool
sl_wisun_ota_dfu_get_fw_update_status_flag(const sl_wisun_ota_dfu_status_t status_flag)

Get the status flag value.

const char *

Get the status string in JSON format.

sl_status_t
sl_wisun_ota_dfu_get_gbl_path(char *const dst_gbl_path, const uint16_t dst_gbl_path_size)

Get GBL file path.

sl_status_t
sl_wisun_ota_dfu_get_host_addr(char *const dst_host, const uint16_t dst_host_size, uint16_t *dst_port)

Get host addres and port.

sl_status_t
sl_wisun_ota_dfu_get_host_uri(char *const dst_uri, const uint16_t dst_uri_size)

Get host uri path.

void

Initialize the device firmware upgrade service.

sl_status_t
sl_status_t
sl_wisun_ota_dfu_set_gbl_path(const char *gbl_path)

Set GBL file path.

sl_status_t
sl_wisun_ota_dfu_set_host_addr(const char *host, const uint16_t port)

Set host address and port.

sl_status_t

Set host uri path.

sl_status_t

Start firmware update.

sl_status_t

Stop firmware update.

Function Documentation#

sl_wisun_ota_dfu_error_hnd#

void sl_wisun_ota_dfu_error_hnd (const sl_wisun_ota_dfu_error_code_t error_code, sl_wisun_ota_dfu_error_ctx_t *const ctx)

OTA DFU error handler (weak implementation)

Parameters
[in]error_code

Error code

[in]ctx

Error context with error details

Catch error in different stages of boot load.


Definition at line 212 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_free_fw_update_status_json_str#

void sl_wisun_ota_dfu_free_fw_update_status_json_str (const char * str)

Free the status string buffer.

Parameters
[in]str

String ptr

Call CoAP free to release allocated memory


Definition at line 196 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_get_fw_update_status#

uint32_t sl_wisun_ota_dfu_get_fw_update_status (void )

Get the status value.

Parameters
N/A

Returning the value of event flags Returns

  • uint32_t Status


Definition at line 182 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_get_fw_update_status_flag#

bool sl_wisun_ota_dfu_get_fw_update_status_flag (const sl_wisun_ota_dfu_status_t status_flag)

Get the status flag value.

Parameters
[in]status_flag

Status flag enum

Bool representation of status variable bit value Returns

  • bool true if the flag is set, otherwise false


Definition at line 204 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_get_fw_update_status_json_str#

const char * sl_wisun_ota_dfu_get_fw_update_status_json_str (void )

Get the status string in JSON format.

Parameters
N/A

String buffer is allocated in heap by CoAP allocator Returns

  • const char * Allocated string pointer on success, otherwise NULL


Definition at line 189 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_get_gbl_path#

sl_status_t sl_wisun_ota_dfu_get_gbl_path (char *const dst_gbl_path, const uint16_t dst_gbl_path_size)

Get GBL file path.

Parameters
[out]dst_gbl_path

GBL file path

[in]dst_gbl_path_size

GBL path size

Get GBL file path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 269 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_get_host_addr#

sl_status_t sl_wisun_ota_dfu_get_host_addr (char *const dst_host, const uint16_t dst_host_size, uint16_t * dst_port)

Get host addres and port.

Parameters
[out]dst_host

Host address

[in]dst_host_size

Host address size

[out]dst_port

Host port

Get host address and port Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 232 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_get_host_uri#

sl_status_t sl_wisun_ota_dfu_get_host_uri (char *const dst_uri, const uint16_t dst_uri_size)

Get host uri path.

Parameters
[out]dst_uri

Uri path

[in]dst_uri_size

Uri path size

Get host uri path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 251 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_init#

void sl_wisun_ota_dfu_init (void )

Initialize the device firmware upgrade service.

Parameters
N/A

Initialize Wi-SUN OTA Device Firmware Upgrade service.


Definition at line 148 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_reboot_and_install#

sl_status_t sl_wisun_ota_dfu_reboot_and_install (void )

Reboot device.

Parameters
N/A

Reboot device with calling corresponding gecko bootloader 'bootloader_rebootAndInstall' API This functions is available if auto-reboot mode is disabled. Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 174 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_set_gbl_path#

sl_status_t sl_wisun_ota_dfu_set_gbl_path (const char * gbl_path)

Set GBL file path.

Parameters
[in]gbl_path

GBL file path

Set GBL file path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 260 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_set_host_addr#

sl_status_t sl_wisun_ota_dfu_set_host_addr (const char * host, const uint16_t port)

Set host address and port.

Parameters
[in]host

Host address

[in]port

Host port

Set host address and port Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 222 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_set_host_uri#

sl_status_t sl_wisun_ota_dfu_set_host_uri (const char * uri)

Set host uri path.

Parameters
[in]uri

Uri path

Set host uri path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 242 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_start_fw_update#

sl_status_t sl_wisun_ota_dfu_start_fw_update (void )

Start firmware update.

Parameters
N/A

Start firmware update by setting SL_WISUN_OTA_DFU_STATUS_FW_UPDATE_STARTED flag Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 156 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

sl_wisun_ota_dfu_stop_fw_update#

sl_status_t sl_wisun_ota_dfu_stop_fw_update (void )

Stop firmware update.

Parameters
N/A

Stop firmware update by setting SL_WISUN_OTA_DFU_STATUS_FW_UPDATE_STOPPED flag Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Definition at line 164 of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h