Wi-SUN OTA DFU download error context definition.
Public Attribute Documentation#
data_size#
uint16_t sl_wisun_ota_dfu_error_ctx_fw_download::data_size
Data size.
Definition at line
113
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h
offset#
uint32_t sl_wisun_ota_dfu_error_ctx_fw_download::offset
Offset of GBL file.
Definition at line
111
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h
ret_val#
int32_t sl_wisun_ota_dfu_error_ctx_fw_download::ret_val
Return value of API call.
Definition at line
109
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h