iPerf Client Isochronus payload

Public Attributes#

uint32_t

period units microseconds

uint32_t

Burst size.

uint32_t

Frame ID.

uint32_t

Previous frame ID.

uint32_t

Remaining.

uint32_t

Reserved.

uint32_t

Start sec.

uint32_t

Start usec.

Public Attribute Documentation#

burst_period#

uint32_t sl_iperf_clnt_hdr_isoch_payload::burst_period

period units microseconds


Definition at line 392 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

burst_size#

uint32_t sl_iperf_clnt_hdr_isoch_payload::burst_size

Burst size.


Definition at line 402 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

frame_id#

uint32_t sl_iperf_clnt_hdr_isoch_payload::frame_id

Frame ID.


Definition at line 400 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

prev_frameid#

uint32_t sl_iperf_clnt_hdr_isoch_payload::prev_frameid

Previous frame ID.


Definition at line 398 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

remaining#

uint32_t sl_iperf_clnt_hdr_isoch_payload::remaining

Remaining.


Definition at line 404 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

reserved#

uint32_t sl_iperf_clnt_hdr_isoch_payload::reserved

Reserved.


Definition at line 406 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

start_tv_sec#

uint32_t sl_iperf_clnt_hdr_isoch_payload::start_tv_sec

Start sec.


Definition at line 394 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

start_tv_usec#

uint32_t sl_iperf_clnt_hdr_isoch_payload::start_tv_usec

Start usec.


Definition at line 396 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h