iPerf connection descriptor type definition
Public Attributes#
uint8_t *
Buffer ptr to receive/transmit.
size_t
RX/TX buffer transmit.
Client sock addr IP.
bool
Server (rx'd) or client (tx'd) started.
int32_t
local socket id
int32_t
Accepted sock used by TCP server to rx.
Server sock addr IP.
Public Attribute Documentation#
buff#
uint8_t* sl_iperf_conn::buff
Buffer ptr to receive/transmit.
Definition at line
208
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
buff_size#
size_t sl_iperf_conn::buff_size
RX/TX buffer transmit.
Definition at line
210
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
clnt_addr#
sl_iperf_socket_addr_t sl_iperf_conn::clnt_addr
Client sock addr IP.
Definition at line
204
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
run#
bool sl_iperf_conn::run
Server (rx'd) or client (tx'd) started.
Definition at line
206
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
socket_id#
int32_t sl_iperf_conn::socket_id
local socket id
Definition at line
198
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
socket_id_clnt#
int32_t sl_iperf_conn::socket_id_clnt
Accepted sock used by TCP server to rx.
Definition at line
200
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
srv_addr#
sl_iperf_socket_addr_t sl_iperf_conn::srv_addr
Server sock addr IP.
Definition at line
202
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h