Configurations#

Macros#

#define

Default notification ID string.

#define

Default remote address to send status report.

#define

Default port of the remote host to send status report.

#define

Default schedule time to send status report.

#define

Default URI Path to use in status report packet.

#define

Enable execution time.

#define
#define

Macro Definition Documentation#

SL_WISUN_APP_STATUS_DEFAULT_NOTIFCATION_ID#

#define SL_WISUN_APP_STATUS_DEFAULT_NOTIFCATION_ID
Value:
"app-status"

Default notification ID string.


Definition at line 58 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_DEFAULT_REMOTE_ADDR#

#define SL_WISUN_APP_STATUS_DEFAULT_REMOTE_ADDR
Value:
"2001:db8::1"

Default remote address to send status report.


Definition at line 50 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_DEFAULT_REMOTE_PORT#

#define SL_WISUN_APP_STATUS_DEFAULT_REMOTE_PORT
Value:
5683U

Default port of the remote host to send status report.


Definition at line 46 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_DEFAULT_SCHEDULE_TIME_MS#

#define SL_WISUN_APP_STATUS_DEFAULT_SCHEDULE_TIME_MS
Value:
10000UL

Default schedule time to send status report.


Definition at line 62 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_DEFAULT_URI_PATH#

#define SL_WISUN_APP_STATUS_DEFAULT_URI_PATH
Value:
"app/status"

Default URI Path to use in status report packet.


Definition at line 54 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_DEVICE_INFO_ENABLE#

#define SL_WISUN_APP_STATUS_DEVICE_INFO_ENABLE
Value:
1U

Enable execution time.


Definition at line 74 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_EXECUTION_TIME_ENABLE#

#define SL_WISUN_APP_STATUS_EXECUTION_TIME_ENABLE
Value:
1U

Enable execution time.


Definition at line 70 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h

SL_WISUN_APP_STATUS_NEIGHBOR_INFO_ENABLE#

#define SL_WISUN_APP_STATUS_NEIGHBOR_INFO_ENABLE
Value:
1U

Enable Neighbor info.


Definition at line 66 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/app/wisun/component/app_status/config/sl_wisun_app_status_config.h