CoAP#

The Wi-SUN CoAP component offers an application layer implementation built on top of the Wi-SUN stack and its socket API. The CoAP protocol is specifically designed as an Internet Application Protocol for constrained devices operating in lossy networks (as defined in RFC 7252). Wi-SUN FAN networks precisely fit this definition.

The CoAP implementation relies on the UDP transport layer for sending and receiving packets. Within the component, you'll find a set of helper functions that assist in building CoAP payloads, parsing CoAP packets, and freeing CoAP packets. Additionally, the CoAP Resource Handler service manages registered resources.

For resource discovery, the Resource Discovery request provides an interface to retrieve information about available resources. These resources have additional attributes beyond the URI (Uniform Resource Identifier) path, which can be selectively filtered using specific Resource Discovery requests.

Furthermore, the CoAP Notification service allows the creation and schedule of notifications for the remote host. The schedule time and send conditions can be customized based on the application requirements. To incorporate the CoAP component into the application, simply add it to the project and initialize it using sl_wisun_coap_init().

The CoAP component is compatible with third-party implementations, such as the libcoap server and client binaries.

The following block diagram shows the architecture of CoAP component: coapcoap

The following example shows the CoAP resource and notification initialization:

#include <string.h>
#include "sl_wisun_coap.h"
#include "sl_wisun_coap_rhnd.h"
#include "sl_wisun_coap_notify.h"

#define NOTIFY_URI_PATH "notify/temperature"

// CoAP Resource Handler callback
static sl_wisun_coap_packet_t *
callback_to_handle_requests(const sl_wisun_coap_packet_t * const req_packet) {
  sl_wisun_coap_packet_t *resp_packet = NULL;

  // Build pre-initialized CoAP packet with content response message code
  resp_packet = sl_wisun_coap_build_response(req_packet, COAP_MSG_CODE_RESPONSE_CONTENT);
  if (resp_packet == NULL) {
    return NULL;
  }

  // Build your CoAP payload (resp_packet->payload_ptr)
  // and set the payload length (resp_packet->payload_len)

  return resp_packet;
}

static bool condition_callback(const sl_wisun_coap_notify_t * notify) {
  // Build your notification condition and return the check result
  (void) notify;
  return true;
}

static sl_wisun_coap_packet_t *
callback_to_build_packet(const sl_wisun_coap_notify_t *notify) {
  // Initialize a CoAP Packet
  static sl_wisun_coap_packet_t pkt = {
    .msg_code = COAP_MSG_CODE_REQUEST_PUT, // Message Code: PUT request
    .msg_id = 1234, // Message ID
    .msg_type = COAP_MSG_TYPE_NON_CONFIRMABLE, // Message type
    .content_format = COAP_CT_TEXT_PLAIN, // Content format
    .uri_path_ptr = NULL, // URI Path pointer
    .uri_path_len = 0, // URI Path length
    .payload_ptr = NULL, // Payload pointer
    .payload_len = 0, // Payload length
    .token_ptr = NULL, // Token pointer
    .token_len = 0, // Token length
    .options_list_ptr = NULL // Option list pointer
  };

  (void) notify;

  // Set the URI path
  pkt.uri_path_ptr = (uint8_t *)NOTIFY_URI_PATH;
  pkt.uri_path_len = strlen(NOTIFY_URI_PATH);

  // Set your notificaiton payload content
  // pkt.payload_ptr = your_prebuilt_buf;
  // pkt.payload_len = your_payload_length;

  // Return with the notification packet
  return &pkt;
}


static void init_resource_and_notification(void) {
  // Return value
  int32_t ret = 0;

  // Resource descriptor allocation
  sl_wisun_coap_rhnd_resource_t coap_resource = { 0 };

  // Notification handler allocation
  sl_wisun_coap_notify_t notify = { 0 };

  // Prepare resource with default content
  sl_wisun_coap_rhnd_resource_init(&coap_resource);

  // Resource URI path
  coap_resource.data.uri_path = "/sensor/temperature";

  // Resource type
  coap_resource.data.resource_type = "temp";

  // Interface
  coap_resource.data.interface = "i2c-sensor";

  // Function pointer to handle requests, like temperature measurement and response packet build.
  // Pointer type is sl_wisun_coap_packet_t * (*)(const sl_wisun_coap_packet_t * const req_packet)
  coap_resource.auto_response = callback_to_handle_requests;

  // You can initialize an extended callback instead of the standard callback type.
  // The extended callback receives the source address of the requests.
  // The function pointer type is
  // sl_wisun_coap_packet_t * (*)(const sockaddr_in6_t * const src_addr, const sl_wisun_coap_packet_t * const req_packet)
  // coap_resource.auto_response_ext = extended_callback_to_handle_requests;

  // Redirect response
  // The callback performs a response redirection. You can build your new destination address
  // and retrieve the new_addr argument
  // Pointer type is
  // void (*)(sockaddr_in6_t * const new_addr,const sl_wisun_coap_packet_t * const req_packet)
  // coap_resource.redirect_response = NULL;

  // Resource is discoverable. You can get information with resource discovery request
  // GET /.well-known/core
  coap_resource.discoverable = true;

  // Add resource to the resource list
  assert(sl_wisun_coap_rhnd_resource_add(&coap_resource) == SL_STATUS_OK);

  // Set the notification ID
  notify.id = "my-notification";

  // Set the destination address of notification
  ret = inet_pton(AF_INET6,
                  "2001:db8::1",
                  &notify.remote_addr.sin6_addr);
  assert(ret == 1);
  notify.remote_addr.sin6_port = htons(5683);

  // Set the schedule time of the notification, 1s is in the example
  notify.schedule_time_ms = 1000;

  // Initialize the condition callback.
  // The callback checks the condition whether the created CoAP packet should be sent
  // The function pointer type is bool (*)(const sl_wisun_coap_notify_t * notify)
  notify.condition_cb = condition_callback;

  // Initialize the notification handler that builds the CoAP packet
  // The function pointer type is
  // sl_wisun_coap_packet_t * (*)(const sl_wisun_coap_notify_t * notify)
  notify.hnd_cb = callback_to_build_packet;

  // Add the notification to the notification list
  assert(sl_wisun_coap_notify_add(&notify) == SL_STATUS_OK);
}

Modules#

Configurations

Type definitions

CoAP Resource Handler API

CoAP Notification API

Functions#

sl_wisun_coap_build_response(const sl_wisun_coap_packet_t *req, sl_wisun_coap_message_code_t msg_code)

Build generic response for request wrapper function.

int16_t
sl_wisun_coap_builder(uint8_t *dest_buff, const sl_wisun_coap_packet_t *message)

CoAP message builder Wi-SUN.

uint16_t
sl_wisun_coap_builder_calc_size(const sl_wisun_coap_packet_t *message)

CoAP packet calc size wrapper.

void
sl_wisun_coap_destroy_packet(sl_wisun_coap_packet_t *packet)

Destroy packet.

__STATIC_INLINE void

Destroy payload string.

__STATIC_INLINE void

Destroy URI path string.

void
sl_wisun_coap_free(void *addr)

Free Wi-SUN CoAP.

Get the library handler pointer from the internal handler structure.

char *
sl_wisun_coap_get_payload_str(const sl_wisun_coap_packet_t *const packet)

Prepare payload string.

char *
sl_wisun_coap_get_uri_path_str(const sl_wisun_coap_packet_t *const packet)

Prepare URI path string.

void
sl_wisun_coap_init(const sl_wisun_coap_tx_callback tx_callback, const sl_wisun_coap_rx_callback rx_callback, const sl_wisun_coap_version_t version)

Initialize Wi-SUN CoAP.

__STATIC_INLINE void

Initialize Wi-SUN CoAP default.

void *
sl_wisun_coap_malloc(uint16_t size)

Implement malloc.

sl_wisun_coap_parser(uint16_t packet_data_len, uint8_t *packet_data)

CoAP parser wrapper function.

void
sl_wisun_coap_print_packet(const sl_wisun_coap_packet_t *packet, const bool hex_format)

Print CoAP packets and all of attached buffer, payload, token, uri_path.

Macros#

#define

CoAP Service loop.

Function Documentation#

sl_wisun_coap_build_response#

sl_wisun_coap_packet_t * sl_wisun_coap_build_response (const sl_wisun_coap_packet_t * req, sl_wisun_coap_message_code_t msg_code)

Build generic response for request wrapper function.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *[in]req

request

sl_wisun_coap_message_code_t[in]msg_code

message code to build

Used sn_coap_build_response. Returns

  • sl_wisun_coap_header_t* built packet ptr on the heap


sl_wisun_coap_builder#

int16_t sl_wisun_coap_builder (uint8_t * dest_buff, const sl_wisun_coap_packet_t * message)

CoAP message builder Wi-SUN.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]dest_buff

destination buffer for raw message

const sl_wisun_coap_packet_t *[in]message

message structure

Used sl_wisun_coap_builder. Returns

  • int16_t On success bytes of built message, on failure -1 if CoAP header structure is wrong -2 if NULL ptr set as argument


sl_wisun_coap_builder_calc_size#

uint16_t sl_wisun_coap_builder_calc_size (const sl_wisun_coap_packet_t * message)

CoAP packet calc size wrapper.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *[in]message

message ptr

Used sn_coap_builder_calc_needed_packet_data_size. Returns

  • uint16_t size


sl_wisun_coap_destroy_packet#

void sl_wisun_coap_destroy_packet (sl_wisun_coap_packet_t * packet)

Destroy packet.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_coap_packet_t *N/Apacket

packet

It must be used to avoid memory leaks! Free the all of allocated buffer for packet


sl_wisun_coap_destroy_payload_str#

__STATIC_INLINE void sl_wisun_coap_destroy_payload_str (char * str)

Destroy payload string.

Parameters
TypeDirectionArgument NameDescription
char *[in]str

String

'\0' terminated string in the heap, it must be freed


sl_wisun_coap_destroy_uri_path_str#

__STATIC_INLINE void sl_wisun_coap_destroy_uri_path_str (const char * uri_str)

Destroy URI path string.

Parameters
TypeDirectionArgument NameDescription
const char *[in]uri_str

URI string ptr

Call free on allocated pointer


sl_wisun_coap_free#

void sl_wisun_coap_free (void * addr)

Free Wi-SUN CoAP.

Parameters
TypeDirectionArgument NameDescription
void *N/Aaddr

address ptr

OS-dependent thread-safe implementation.


sl_wisun_coap_get_lib_handler#

const sl_wisun_coap_handle_t * sl_wisun_coap_get_lib_handler (void )

Get the library handler pointer from the internal handler structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Not thread safe! It is needed only to use Pelion mbed-coap library functions Returns

  • const sl_wisun_coap_handle_t* pointer to the lib handler


sl_wisun_coap_get_payload_str#

char * sl_wisun_coap_get_payload_str (const sl_wisun_coap_packet_t *const packet)

Prepare payload string.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *const[in]packet

Packet

'\0' terminated string in the heap, it must be freed Returns

  • char* payload string, NULL on error


sl_wisun_coap_get_uri_path_str#

char * sl_wisun_coap_get_uri_path_str (const sl_wisun_coap_packet_t *const packet)

Prepare URI path string.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *const[in]packet

Packet

'\0' terminated string in the heap, it must be freed Returns

  • char* URI path string, NULL on error


sl_wisun_coap_init#

void sl_wisun_coap_init (const sl_wisun_coap_tx_callback tx_callback, const sl_wisun_coap_rx_callback rx_callback, const sl_wisun_coap_version_t version)

Initialize Wi-SUN CoAP.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_tx_callback[in]tx_callback

TX callback, if it's NULL, the default callback is applied

const sl_wisun_coap_rx_callback[in]rx_callback

RX callback, if it's NULL, the default callback is applied

const sl_wisun_coap_version_t[in]version

CoAP version

Set the Wi-SUN CoAP internal descriptor.


sl_wisun_coap_init_default#

__STATIC_INLINE void sl_wisun_coap_init_default (void )

Initialize Wi-SUN CoAP default.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initializes the internal descriptor with default values.


sl_wisun_coap_malloc#

void * sl_wisun_coap_malloc (uint16_t size)

Implement malloc.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Asize

size for malloc

OS-dependent thread-safe implementation. Returns

  • void* the memory pointer


sl_wisun_coap_parser#

sl_wisun_coap_packet_t * sl_wisun_coap_parser (uint16_t packet_data_len, uint8_t * packet_data)

CoAP parser wrapper function.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]packet_data_len

packet data size

uint8_t *[in]packet_data

packet data ptr

Used sn_coap_parser Returns

  • sl_wisun_coap_packet_t* Parsed packet pointer


sl_wisun_coap_print_packet#

void sl_wisun_coap_print_packet (const sl_wisun_coap_packet_t * packet, const bool hex_format)

Print CoAP packets and all of attached buffer, payload, token, uri_path.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *[in]packet

packet to print

const bool[in]hex_format

hex format bool to decide buffer print format

Pretty printer function, with hex format option for buffers


Macro Definition Documentation#

SL_COAP_SERVICE_LOOP#

#define SL_COAP_SERVICE_LOOP
Value:
()

CoAP Service loop.