Indication message body.

Public Attributes#

uint32_t

Bit mask indicating the changes.

uint32_t

Status of the indication.

Public Attribute Documentation#

flags#

uint32_t sl_wisun_msg_network_update_ind_body_t::flags

Bit mask indicating the changes.


Definition at line 159 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

status#

uint32_t sl_wisun_msg_network_update_ind_body_t::status

Status of the indication.


Definition at line 154 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h