Indication message body.
Public Attributes#
uint8_t
Received data.
uint16_t
Amount of received data.
IP address of the sender.
uint16_t
Port number of the sender.
int32_t
ID of the socket.
uint32_t
Status of the indication.
Public Attribute Documentation#
data#
uint8_t sl_wisun_msg_socket_data_ind_body_t::data[]
Received data.
Definition at line
194
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
data_length#
uint16_t sl_wisun_msg_socket_data_ind_body_t::data_length
Amount of received data.
Definition at line
192
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
remote_address#
in6_addr_t sl_wisun_msg_socket_data_ind_body_t::remote_address
IP address of the sender.
Definition at line
188
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
remote_port#
uint16_t sl_wisun_msg_socket_data_ind_body_t::remote_port
Port number of the sender.
Definition at line
190
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
socket_id#
int32_t sl_wisun_msg_socket_data_ind_body_t::socket_id
ID of the socket.
Definition at line
186
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
status#
uint32_t sl_wisun_msg_socket_data_ind_body_t::status
Status of the indication.
Definition at line
184
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h