Indication message body.

Public Attributes#

int32_t

ID of the socket.

uint32_t

Amount of free space in the transmission buffer.

uint32_t

Status of the indication.

Public Attribute Documentation#

socket_id#

int32_t sl_wisun_msg_socket_data_sent_ind_body_t::socket_id

ID of the socket.


Definition at line 383 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

socket_space_left#

uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::socket_space_left

Amount of free space in the transmission buffer.


Definition at line 385 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

status#

uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::status

Status of the indication.


Definition at line 381 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h