iPerf Client Isochronus settings

Public Attributes#

int32_t

Lower Burst IPG.

int32_t

Lower FPS.

int32_t

Lower Mean.

int32_t

Lower Variance.

int32_t

Upper Burst IPG.

int32_t

Upper FPS.

int32_t

Upper Mean.

int32_t

Upper Variance.

Public Attribute Documentation#

l_burst_ipg#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::l_burst_ipg

Lower Burst IPG.


Definition at line 442 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_fps#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::l_fps

Lower FPS.


Definition at line 430 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_mean#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::l_mean

Lower Mean.


Definition at line 434 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_variance#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::l_variance

Lower Variance.


Definition at line 438 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_burst_ipg#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::u_burst_ipg

Upper Burst IPG.


Definition at line 444 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_fps#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::u_fps

Upper FPS.


Definition at line 432 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_mean#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::u_mean

Upper Mean.


Definition at line 436 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_variance#

int32_t sl_iperf_clnt_hdr_ext_isoch_settings::u_variance

Upper Variance.


Definition at line 440 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h