Confirmation message body.

Public Attributes#

uint16_t

Size of the routing table.

uint8_t

Reserved, set to zero.

uint32_t

Status of the request.

Public Attribute Documentation#

entry_count#

uint16_t sl_wisun_br_msg_get_routing_table_entry_count_cnf_body_t::entry_count

Size of the routing table.


reserved#

uint8_t sl_wisun_br_msg_get_routing_table_entry_count_cnf_body_t::reserved[2]

Reserved, set to zero.


status#

uint32_t sl_wisun_br_msg_get_routing_table_entry_count_cnf_body_t::status

Status of the request.