Request message body.

Public Attributes#

uint8_t

True to start PAN Defect procedure, false to stop it.

uint32_t

Duration after which devices should systemically switch to the alternative PAN if one is available.

uint32_t

Minimum duration after which devices are allowed to switch their PAN if an alternative one is available.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

defect_advertise#

uint8_t sl_wisun_br_msg_pan_defect_advertise_req_body_t::defect_advertise

True to start PAN Defect procedure, false to stop it.


max_scan_duration_s#

uint32_t sl_wisun_br_msg_pan_defect_advertise_req_body_t::max_scan_duration_s

Duration after which devices should systemically switch to the alternative PAN if one is available.


min_scan_duration_s#

uint32_t sl_wisun_br_msg_pan_defect_advertise_req_body_t::min_scan_duration_s

Minimum duration after which devices are allowed to switch their PAN if an alternative one is available.


reserved#

uint8_t sl_wisun_br_msg_pan_defect_advertise_req_body_t::reserved[3]

Reserved, set to zero.