Request message body.

Public Attributes#

uint8_t

(L)GTK to install after revocation

uint8_t

Reserved, set to zero.

uint8_t

Revokes GTKs when set to 0, and LGTKs otherwise.

uint8_t

True to use hardcoded GTK, false to generate a random one.

Public Attribute Documentation#

hardcoded_gtk#

uint8_t sl_wisun_br_msg_revoke_gtks_req_body_t::hardcoded_gtk[SL_WISUN_GTK_LEN]

(L)GTK to install after revocation


reserved#

uint8_t sl_wisun_br_msg_revoke_gtks_req_body_t::reserved[2]

Reserved, set to zero.


revoke_lgtks#

uint8_t sl_wisun_br_msg_revoke_gtks_req_body_t::revoke_lgtks

Revokes GTKs when set to 0, and LGTKs otherwise.


use_hardcoded_gtk#

uint8_t sl_wisun_br_msg_revoke_gtks_req_body_t::use_hardcoded_gtk

True to use hardcoded GTK, false to generate a random one.